Posts Tagged ‘Sale’

Give an I-Sobot for the Holidays!

Wednesday, December 17th, 2008

When we announced that we would be cutting the I-Sobot’s price in half, making it only $95.99, our initial pre=orders sold out before we even got the shipment in! We’ve just received another shipment, so if you’re looking for an awesome hi-tech holiday gift for a geek near you (Here’s looking at you kid), this is the perfect choice! This robot debuted on the market at $300, so this is a killer deal!

What’s an I-Sobot? Well he’s the tiniest humanoid robot in production! The ultimate desk toy, this little robot stands only 6.5″ tall but is articulated as most larger humanoid bots with 17 servos, as well as voice commands, remote control, and over 100 special actions and dance routines!  If you order one soon there is still time to get it in before Christmas.

Big Blue Saw’s End of the Year Sale!

Monday, December 15th, 2008

Our friends over at Big Blue Saw are having another sale, which is pretty much a dream come true for Roboticists building their own bots. They are generously offering discount quantity pricing on as little as single part orders, which means major savings for anyone looking to get custom work done for their projects. If you’ve ever looked into machine shop pricing you’ll know what a fantastic deal this is, you won’t find pricing like this anywhere so be sure to check them out! Founder Simon Arthur explains the details:

Big Blue Saw’s latest sale starts Tuesday, December 16, 2008 and ends Tuesday, January 6, 2009.

With this sale any aluminum 6061 parts of 0.1 inch or 0.063 inch thickness are automatically automatically eligible for a quantity discount — even on orders of as little as one part!

This is an excellent opportunity to try our services — you can order just one small part, and save on the setup charges.

This offer is valid for orders placed through our online ordering system only.

About the materials

Aluminum 6061

One of the perennial favorite materials at Big Blue Saw, the 6061 alloy of aluminum features excellent strength and light weight. It is weldable and has good corrosion resistance. This alloy is a true “aircraft aluminum”. Among many other applications, it was chosen by NASA to construct the crew cabin of the Space Shuttle.