Posts Tagged ‘Robotis’

RX-64: Just one more weapon in Skynet’s arsenal

Thursday, April 30th, 2009

I remember being blown away at how strong my first hobby servos were when I built my Hexapod 2 from Lynxmotion about 12 years ago. In comparison, they were literally just a fraction of the strength of modern digital servos, and the gap widens even further when put up against a robotic actuator such as the RX-64 Smart Actuator.

I was working on my mech Hagetaka the other night and made the mistake of grabbing at the robot to stabilize it while it was moving, and managed to graze my finger in one of the joints. It drew blood and immediately reminded me that working with these types of servos was an entirely different ballgame than your standard hobby servo. With that in mind, we put together a little demonstration video of just how powerful these servos can be! Enjoy!

Robotis Ollo Bug Kit

Thursday, April 23rd, 2009

OLLO is a reconfigurable robot construction kit for beginners of any age. Using an easy to build plates and rivets system you’ll be on your way to making your own robot in no time! The OLLO Bug Kit has very detailed and well illustrated instructions to build 4 different types of robotic bugs that can trace lines, detect objects, or be controlled via wireless remote. The modular and simple building system allows you to build custom robots very quickly; your imagination is the limit!

Hagetaka: A Bipedal Combat Robot

Thursday, April 16th, 2009

Remember when we teased you with a stack of RX-64 servos? Well its time to unveil a bit more of what we’re working on for the upcoming Mech Warfare competition at Robogames 2009. Meet Hagetaka; a 7DOF per leg biped built around the powerful RX-64 servo from Robotis. This robot boasts 14 RX-64s, 2 RX-28s, a custom aluminum chassis machined by sponsor Big Blue Saw, an onboard linux based Gumstix computer with a PS3 Sixaxis controller , a WiFi video server using a Headplay Personal Cinema System for remote piloting, and of course dual automatic airsoft guns. Video and more info will be available in the near future, and be sure to check out the June issue of SERVO magazine for the first in a series of articles detailing the build process of this Mech.

Click for larger image.

New parts are in the house!

Wednesday, April 8th, 2009
We have more goodies in and cannot wait to share! We’re serious, it’s like Christmas morning each day we get new stuff in, just ask our extremely annoyed shipping/receiving department about it. New product shows up and our techs swarm in like vultures!
First up we have the Propeller Education Kit which is an absolute steal at $99.99. Included is everything you need to get started using Parallax’s very capable Propeller microcontroller technology. Why use a normal microcontroller when you can get 8 of them in a single chip? Included in the kit is a Propstick USB, a Propeller Fundamentals Lab/Project book, various components needed for said projects, and some neat interconnecting breadboards for rapid prototyping.
Propeller
We’re also proud to introduce our new Mosquit-IO Pan/Tilt kit! The Mosquit-IO is a board we had custom designed specifically to answer the call of a low cost pan/tilt controller, bringing the price down $20 from our previous Pan/Tilt Kit. The Mosquit-IO can control two servos and a 6v DC motor, and is also available separately. A USB interface, simple command syntax, and provided .NET example code make this very easy to get up and running.
mosquit IO
Drooling over the insane torque and features of the DX-117, RX-28, RX-64 Robot servos from Robotis? We are too, and we’re making it even easier to implement them into your next project by offering a High Quality Aluminum bracket system for these. Hinge brackets, side brackets, bearing hubs, and thrust bearings! Everything you need to get started in building the ultimate high torque robot!
of-64h

Want to win a Bioloid? Announcing the TRC Tutorial Contest!

Friday, March 27th, 2009
Time flies! It’s that time again to officially announce the next round of the Trossen Robotics Community (TRC) Contest. We had quite a bit of success with our previous Project Contests and a lot of very cool entries, however we are going to mix things up this time.
This round is going to be a Tutorial Contest , and is quite a bit different from our previous contests. Think of it as an ‘Instructables meets How Stuff Works’ style contest: We want you to submit entries in the form of a detailed step by step ‘How-To’ or Informative Tutorials.
We’re going to be asking a lot more of our participants this round, so we have raised the stakes and are giving away our biggest prizes yet! Without further ado here are the prizes being offered for this round!
1st place

bioloid


Bioloid Comprehensive Kit:


2nd place



Bioloid Beginner Kit:


3rd place


ollo


Robotis Ollo Bug Kit
:

  • New Beginner Robotics Kit from Robotis!
  • Reconfigurable, modular design
  • Tons of parts to build with!
  • Instructions to build 4 different robots included
  • Remote controlled
  • Highly descriptive well documented instructions


You’re probably asking: “Well what’s the catch?” We won’t lie, we’re going to make you work for it and put your knowledge to the test!

Here are some examples of what types of tutorials we’re looking for:

  • What is a gyroscope/accelerometer/analog or digital signal?
  • How do servos/DC Motors/Batteries work? (explain inner workings, control, show example code, etc)
  • Choosing the right (Microcontroller/DC Motor/Sensor) for the job.
  • How to setup an Arduino/Xbee Communication/Basic Stamp. (basic projects with example code, videos, etc)
  • How to control a robot wirelessly. (many different methods of going about this, pick one and elaborate!)
  • Theory of Inverse Kinematics, Dead Reckoning, Spacial Mapping, etc.
We’re looking for well written, detailed entries that a beginner could read through and learn from. The emphasis on this is creating valuable tutorials and FAQs that the community as a whole can benefit from. Diagrams, pictures, source code, practical applications, text references and examples are welcomed and strongly encouraged. Plagiarism will not be tolerated, please cite any reference materials used. We are not looking for build articles during this round.
Entries will also be judged in a different manner than before: Contestants are encouraged to post as many tutorials as they like; in fact, the more tutorials submitted, the more points they receive towards their final score. Now that said, quality is greatly valued over quantity. One detailed, well written tutorial will hold more weight than five mediocre ones, but if you post numerous well written tutorials you’re going to be in very good shape.

Previous project submissions were based out of our Project Showcase forum, but this time all submissions must be entered into the Tutorial section.

Please visit our Project Contest Page to learn more about the contest, how to enter and for the official rules and guidelines. Somebody is going to be a proud new owner of a Bioloid Comprehensive Kit, Bioloid Beginner Kit, or Ollo Bug Kit, will it be you?

RX-64s are crazy strong…

Monday, February 23rd, 2009

Our good friend Jon Hylands (who is an amazing Roboticist, definitely check out his work on the Bioloid system) is working on a few new projects and shot a quick video which is pretty impressive to anyone who has ever built a robotics arm. What you see in the video below is an RX-64 Robotis servo lifting a full coke can at a 30 cm arm length. While that seems trivial to we humans, packing that much torque into such a tiny servo is a great demonstration of how much servo technology has advanced in the last few years. The servo isn’t even being strained during these tests. You might note a bit of jerky movement, that is because the servo is being manually fed positional instructions via a slider bar. Most advanced robots use some form of interpolation which smooths movements considerably.

We’ll also be revealing our big internal project which uses 14 of the RX-64 servos in the near future… =)