Posts Tagged ‘RobotGeek’

RobotGeek Sensors and Boards Videos

Tuesday, June 25th, 2013

Not a huge deal, so no need to get hyper or anything. But we posted some new short videos on the Robot Geek Arduino-Compatible Sensors.

Some things that are cool about the Robot Geek Sensors are:

  • Simple normal 3 pin connectors! No fancy special cables needed to plug them in.
  • Standard hole patterns. Most of our sensors are on a 2 X 3cm pattern and anything that isn’t is still on a 1cm x 1cm grid. Logical right?
  • We go further! Need an LED board? You get a board with two connectors (horz & vert) and FIVE colors of LEDs. Not one soldered to the board. FIVE. We don’t know how you want to mount this thing or what color you may want. What if you change your mind too? Here, take five colors. Just don’t hurt us. Or yourself.
  • Cross compatible with all the other systems out there, Phidgets, Seeed Grove, Seeed Brick…


Loading the player…

 

New RobotGeek Voltage Dividers are in the Store!

Wednesday, August 8th, 2012

RobotGeek Voltage Divider

Developed in-house, the RobotGeek Voltage Divider is a great little board that will make it easy to connect analog sensors up to our Arduino. Just about any analog sensor, like out Force, pressure, and flex sensors can be used with the Voltage Divider.

The three pin voltage divider can easily connect directly to the arduino, or attached to a breakout shield. Your sensor can connect to the voltage divider using the 2-pin male header, or the screw terminals. Finally, the built in potentiometer will let you adjust the circuit’s sensitivity.

Check out the product page for a wiring diagram and PCB files.

New Solenoids are Here!

Thursday, July 12th, 2012

Coils are awesome. Ignition coils, Tesla Coils and Coilguns to name a few. But our new favorite coils are the ones in our New Solenoids. These solenoids will move their shaft in and out as you apply a voltage to them – they’re incredibly easy to use and amazingly useful for projects ranging from locking mechanisms to home brew pinball machines.

The smallest solenoid can fit into the tiniest of project boxes, while the largest one can move a whopping 7.5 lbs. And right in between, the medium solenoid is a great compromise between size and strength. We have a Strength Chart of all the solenoids at different voltages, as well as technical drawings and 3D .stp files available on the product pages.

Check our video for more information and to see the incredible feats of strength these solenoids can perform.