Our good friend Jon Hylands (who is an amazing Roboticist, definitely check out his work on the Bioloid system) is working on a few new projects and shot a quick video which is pretty impressive to anyone who has ever built a robotics arm. What you see in the video below is an RX-64 Robotis servo lifting a full coke can at a 30 cm arm length. While that seems trivial to we humans, packing that much torque into such a tiny servo is a great demonstration of how much servo technology has advanced in the last few years. The servo isn’t even being strained during these tests. You might note a bit of jerky movement, that is because the servo is being manually fed positional instructions via a slider bar. Most advanced robots use some form of interpolation which smooths movements considerably.
We’ll also be revealing our big internal project which uses 14 of the RX-64 servos in the near future… =)