Posts Tagged ‘Mech Wars’

Matt Bauer joins the Mech Wars fray, debuts new Mech Combat Platform Software

Tuesday, September 16th, 2008

Matt Bauer, the man behind one of the top Robo-One class humanoid robots in the United States, Rook’s Pawn 3, sat in on the initial pitch and discussion of the Mech Wars event. He was intrigued, but when I asked him what he was planning he kept pretty quiet and simply said he’d release it when it was ready.

Well, Matt did not disappoint. He recently debuted his custom Mech Puppeteer Combat Platform, which is a very slick looking GUI built specifically to control Matt’s soon to be announced Robonova based robot for Mech Wars. Take a gander at the layout and you’ll see what I’m talking about:

Mech Puppeteer Combat Platform
Click to Enlarge.

The buttons light up, weapon systems have animated safety switch features, and a video feed with targeting reticle is built in. These controls are keyboard mappable and Matt is working to make this software as modular as possible and available for public release. Here’s a video showcasing some of the features:

And here’s a short video showing the built in safety features and weapon system of the software:

I personally can’t wait to see what Matt has up his sleeve as far as his actual Mech. If the quality of his software and Rook’s Pawn 3 is any indication, Mech Wars participants are going to be facing some fierce competition from him.