We’ve been busily preparing for the iHobby 2009 show this week, but I figured I would share a little demo video of Giger. He now sports a TinyCylon eye from DaleWheat.com, and has a few new fighting moves up his sleeve, ready for some fights at Chibotica during iHobby! Walking gait is still obviously a work in progress, but what is being demonstrated in the video is the ability to pan/tilt the torso while walking, which makes the walking gait even more unsteady. Enough jabbering, here’s a bit of video!
Posts Tagged ‘Mech Warfare’
Giger is ready for iHobby!
Wednesday, October 21st, 2009Matt Trossen, Hagetaka, and Roboard Featured in Make Magazine
Monday, September 21st, 2009This month’s Make Magazine (Issue 19) is the yearly Robotics Hobbyist special, and features my boss Matt Trossen once again stealing all of my glory and talking about his take on the current state of hobby robotics. That is okay however, and I’m prepared to take it with stride because anyone reading this blog knows I’m the true brains behind this operation. Not only that, but I’m also better looking (it’s the beard) and I embrace an air of dignity and modesty.
Speaking of my dashing good looks and superior mental prowess; Make also featured my currently shelved and ego-crippling project Hagetaka. Rest assured; my wife and 2 year old have picked up 2nd jobs to fund this project further and it will return with even stronger servos and bigger guns, ready to assist me in my plan for world domin- err, winning Mech Warfare.
Last but not least, Make Magazine readers got a quick and to the point review of the Roboard, the first full featured Robotics Computer on the market.
But seriously, be sure to pick up a copy as the entire issue is full of fun projects and robotic tidbits sure to appeal to your average robot-geek. And like Christmas, it only comes once a year!
iPhone controlled Mech?
Thursday, July 2nd, 2009After Year 1 of Mech Warfare, the competitors are busy working away to improve their bots, control scheme, weapons, etc… so it was only a matter of time before we would see someone adapting an iPhone to control their mech. Seeing as though the iPhone can be used for anything (Defibbing people, saving kittens from trees, backup generator for your house, etc), remotely controlling walking combat robots was the next logical step.
Builder Mannyr7 and his mech project CLYDE suffered some last minute setbacks that prevented him from competing at Year 1 (though he did show up to cheer us on and impress us with his professional airsoft gun setup), however he has taken the time to write up a tutorial and shoot a video on his latest iPhone control scheme. Definitely check it out, as its applicable to a variety of robots!
Initial Mech Warfare Coverage
Tuesday, June 23rd, 2009We want to apologize for being so quiet, but Robogames and the subsequent chaos of getting caught up has taken us all by a storm. We’ll be making up for it by posting a ton of content in the next few days.
Year 1 of Mech Warfare turned out great, better than expected for a first year competition. We came, we conquered, and more than anything we learned a LOT. Seven robots total showed up, though Murphy’s Law was in full effect and we only had 4 running consistently. That said, everyone involved still had a ton of fun, and Botjunkie and Society of Robots were there covering the action. Here are two quick highlight videos they put together, stay tuned for the official Mech Warfare coverage video from multiple in-arena cameras in the near future!
Video coverage from Botjunkie:
And video coverage from Society of Robots:
Hagetaka: A Bipedal Combat Robot
Thursday, April 16th, 2009Remember when we teased you with a stack of RX-64 servos? Well its time to unveil a bit more of what we’re working on for the upcoming Mech Warfare competition at Robogames 2009. Meet Hagetaka; a 7DOF per leg biped built around the powerful RX-64 servo from Robotis. This robot boasts 14 RX-64s, 2 RX-28s, a custom aluminum chassis machined by sponsor Big Blue Saw, an onboard linux based Gumstix computer with a PS3 Sixaxis controller , a WiFi video server using a Headplay Personal Cinema System for remote piloting, and of course dual automatic airsoft guns. Video and more info will be available in the near future, and be sure to check out the June issue of SERVO magazine for the first in a series of articles detailing the build process of this Mech.
Luckily, Sarah Conner hasn’t shown up yet
Monday, January 26th, 2009But we’re preparing for when she shows up to blow us away, because this might very well be the start of Skynet.
Robot pr0n warning. (Click for a larger picture)
Well, at least nobody can accuse us of under-engineering. Yup, that’s a pyramid of RX-64s. This is a teaser photo of a new project brewing in the Trossen Robotics Lab for the upcoming Mech Warfare competition. A fully custom aluminum frame and bracket system is being machined courtesy of Big Blue Saw, our sponsor on the project. Did we mention we’re giving it weapons? /snicker
Mech Warfare Featured in Issue 15 of Robot Magazine!
Friday, January 16th, 2009The Mech Warfare competition, which was founded right here at the Trossen Robotics Community (TRC), continues to gain momentum as we count down the months until the debut at Robogames 2009 this summer. Our friends over at Robot Magazine had caught word of the competition, as well as the viral excitement of the builders involved, and asked me to write up an article outlining the competition, the rules, and the participants and their Mechs.
For those of you who may not have heard of Mech Warfare yet, it is a robotic competition in which participants construct remotely piloted walking robots armed with airsoft guns and other weapons to duke it out in an urban style arena. Think of it as small scale R/C MechWarrior.
If you’d like to check out the article, you can pick up the current issue of Robot Magazine in most major bookstores or order it online from our store. For more information on the Mech Warfare event, check out the Official Site and the Mech Warfare Forums. We hope to see you and your Mech at Robogames 2009!