Posts Tagged ‘kickstarter’

DynamixShield Kickstarter!

Wednesday, November 18th, 2015

DynamixShield

Our friend at NeuroRobotic Technologies has been developing an Arduino Due Shield that plays nice with everything in the InterbotiX and RobotGeek product lines (and subsequently, his PhantomX Hexapod is playing nicely with the kids)! This is a comprehensive shield that lets you connect AX, MX, and XL Dynamixel Servos! The DynamixShield is an electronics board that fits onto an Arduino Due microcontroller to give you the ability to control Dynamixel smart servos and regular servos, while also providing numerous Grove and RobotGeek connectors. Grove and RobotGeek are hardware frameworks for modular sensors and actuators. There are tons of off-the-shelf modules for these two frameworks that can be plugged into the shield with a single cable. This includes everything from GPS sensors, RFID scanners, and LCD displays that are plug-and-play ready for use with the shield. This makes it very easy to build your robots by combining modules and servos. Check out his Kickstarter, and if you want to see it happen, you can make it happen!

C.H.I.P. Looks Promising!

Wednesday, May 13th, 2015

Rhoeby

Trossen Robotics is backing CHIP – The World’s First Nine Dollar Computer, for its potential to increase the accessibility of smart, powerful robotics projects to students and roboticists of all ages and levels of expertise. This kickstarter broke a million dollars in the first few days, with a goal of only 50k! The C.H.I.P. is a small form factor, single board computer, much like the Raspberry Pi. It is similarly featured, but diverges in a few important aspects. It has onboard storage of 4GB, built-in WiFi and Bluetooth communications, and a smaller footprint, afforded by the optional VGA and HDMI adapters. There are 23 days left to back this project, so strike while the iron is hot!

RK-1, a wifi Arduino mobile robot for iOS & Android devices

Wednesday, June 5th, 2013

Today’s Kickstarter shout out is for RK-1, an adorable wifi arduino bot to be controlled by smart phones and tablet devices.

From the project page:

The RK-1 is a fun mobile robot, that uses an ad hoc wifi connection, which is controlled using your iOS or Android device.

The control board on the robot is built on the Arduino hardware/software architecture, which is open source, and the controller software and hardware will also be available open source. The idea is to give the community the ability to make Arduino projects mobile. There is no end to what you can do- you can add sensors and actuators to this fun little device and control it remotely.

I have implemented a new and amazing way of controlling the robot using swipe gestures.

RK-1, a wifi Arduino mobile robot for iOS & Android devices