We’ve got you covered. The Acroname 84 Channel USB Servo Controller allows you to control an almost absurd amount of servos making this the perfect board for any over-achiever’s robotics project. Now if controlling 84 servos wasn’t enough, get this: Each of the 84 channels can be set to Digital Input, Digital Output or Servo Output. Additionally, 36 of the channels can act as 10-bit Analog inputs. That makes this one of our most versatile I/O boards yet!
Posts Tagged ‘Controller’
Need to Control a Ridiculous Amount of Servos?
Tuesday, December 9th, 2008Now Taking Pre-Orders on the Bioloid Boomerang ZigBee Controller!
Wednesday, October 22nd, 2008Bioloid users have been drooling over these controllers since they were first announced at Robogames 2008! Well, the time is nigh to get your robot a fix, the Bioloid Boomerang Zigbee Controllers are due on our next shipment! These controllers finally put wireless Bioloid control into user’s hands, enabling easier participation in humanoid kung-fu, soccer, and stairclimbing.
We are now accepting Pre-Orders, with an expected arrival date of November 15th, 2008. They come in two flavors, one with a set of Zig-100s, and one without (if you already had purchased a pair previously). Get em while they’re hot!