Posts Tagged ‘big blue saw’

This Thing Twinges My Geek-DAR Something Fierce

Monday, August 24th, 2009

AwesomeQuad

The creator doesn’t have a name for it past “Little Walking Robot”, but I could think of a few words to describe it: Awesome, sexy, and umm, Awesome.

No but really, thing thing is a marvel of aesthetic design and function. Has a Steampunk meets “Dragoon from Starcraft” look to it. The inventor of this beauty has a well written blog detailing his progress and some of the problems he ran into along the way, as well as a Flickr photo set. This bot is all custom built from a mix of hand-built parts, as well as some waterjet steel frame components from our friends at Big Blue Saw.


Check the video below for the bot in action, big thanks to Big Blue Saw for the scoop.

Hagetaka: A Bipedal Combat Robot

Thursday, April 16th, 2009

Remember when we teased you with a stack of RX-64 servos? Well its time to unveil a bit more of what we’re working on for the upcoming Mech Warfare competition at Robogames 2009. Meet Hagetaka; a 7DOF per leg biped built around the powerful RX-64 servo from Robotis. This robot boasts 14 RX-64s, 2 RX-28s, a custom aluminum chassis machined by sponsor Big Blue Saw, an onboard linux based Gumstix computer with a PS3 Sixaxis controller , a WiFi video server using a Headplay Personal Cinema System for remote piloting, and of course dual automatic airsoft guns. Video and more info will be available in the near future, and be sure to check out the June issue of SERVO magazine for the first in a series of articles detailing the build process of this Mech.

Click for larger image.

Big Blue Saw’s End of the Year Sale!

Monday, December 15th, 2008

Our friends over at Big Blue Saw are having another sale, which is pretty much a dream come true for Roboticists building their own bots. They are generously offering discount quantity pricing on as little as single part orders, which means major savings for anyone looking to get custom work done for their projects. If you’ve ever looked into machine shop pricing you’ll know what a fantastic deal this is, you won’t find pricing like this anywhere so be sure to check them out! Founder Simon Arthur explains the details:

Big Blue Saw’s latest sale starts Tuesday, December 16, 2008 and ends Tuesday, January 6, 2009.

With this sale any aluminum 6061 parts of 0.1 inch or 0.063 inch thickness are automatically automatically eligible for a quantity discount — even on orders of as little as one part!

This is an excellent opportunity to try our services — you can order just one small part, and save on the setup charges.

This offer is valid for orders placed through our online ordering system only.

About the materials

Aluminum 6061

One of the perennial favorite materials at Big Blue Saw, the 6061 alloy of aluminum features excellent strength and light weight. It is weldable and has good corrosion resistance. This alloy is a true “aircraft aluminum”. Among many other applications, it was chosen by NASA to construct the crew cabin of the Space Shuttle.

Big Blue Saw: A Machine Shop for Roboticists!

Monday, November 17th, 2008

A challenge many roboticists and experimenters face is finding a way to get custom metal parts built for their projects. Not everyone can afford to invest thousands of dollars into tools, which is where Big Blue Saw can help. They specialize in custom laser cutting and waterjet machining, and allow builders to place small orders to avoid the high minimum order amounts that most local shops charge.

Big Blue Saw founder and fellow roboticist, Simon Arthur, has been kind enough to give our community the ‘heads up’ when Big Blue Saw is offering specials. We wanted to let all the ‘bot builders out there know about their current sale!

Announcing: Big Blue Saw’s pre-Thanksgiving Sale

From November 20 to November 25, 2008 Big Blue Saw will be having a pre-Thanksgiving sale. Customers will receive quantity discounts on parts made from select materials.

* Aluminum 5052 alloy, 0.08″ thickness
* Aluminum 6061 alloy, 0.125 inch (⅛”) thickness
* Cold roll 1018 carbon steel, 0.125 inch (⅛”) thickness

Any order of less than 10 parts will automatically be eligible for a quantity discount.

Many of you are visiting our website for the first time due to the buzz around the web about this sale. This is an excellent opportunity to try our services — you can order just one small part, and save on the setup charges.
About the materials
Aluminum 6061

One of the perennial favorite materials at Big Blue Saw, the 6061 alloy of aluminum features excellent strength and light weight. It is weldable and has good corrosion resistance. This alloy is a true “aircraft aluminum” and is often used in airplanes and spacecraft.
Aluminum 5052

We have recently added 5052 alloy aluminum as a new standard material here at Big Blue Saw in order to meet the needs of our customers who needed an aluminum alloy that is much easier to bend and form than 6061. It also has good weldability and excellent corrosion resistance.
Cold roll 1018 carbon steel

This carbon steel helps in situations where you need greater strength than aluminum can provide. It has good weldability and will wear better than aluminum.