Cart/Login/Help Tutorials Blog Community Contact
Become an Affiliate!

Archive for the ‘Front Page News’ Category

HUV Bioloid Accessories: Add Sensors to Bioloid!

Tuesday, May 6th, 2008

We’re big fans of the Bioloid system.  We love the smart actuators and integrated sensor modules, but like many Bioloid users, we’ve lamented the lack of additional sensor inputs.  Luckily for us, Bioloid guru Jon Hylands felt the pain of the Bioloid community and created some devices to fill the void.  Thanks to Robotis’ published Dynamixel architecture, anyone who’s savvy with microcontrollers can create peripherals that will blend seamlessly with the stock Bioloid components.  Jon is as savvy as anyone, and we’re happy to be using and selling the hardware he’s created.  Anyway, here’s some cool stuff for all you Bioloid fans out there, or anyone interested in using Dynamixels in their own custom project.

USB Bus Board  
The USB Bus Board gives you virtual COM port access to the Dynamixel serial bus.  It has six connectors, but of course it supports a network of up to 254 Dynamixels.  It uses the FTDI transceiver chip, so if you’ve used other USB virtual COM port devices, there’s a good chance you already have the driver installed.  A great plug-and-play alternative to the USB2Dynamixel adapter.
 
Bioloid I/O Board  
This general-purpose I/O board gives your Bioloid robot the ability to connect to almost any analog (0-5 volt) sensor. It includes 6 analog inputs (10 bit resolution on each). It also includes four general digital I/O pins, and can control one or two DC motor controllers using either locked anti-phase or sign magnitude PWM.  Pretty cool.
 
Bioloid IMU  
In one package, you get 3 axes of acceleration measurement and 3 axes of gyroscopic measurement. It comes fully assembled, and ready to install into a stock Bioloid humanoid chest compartment.
 
FSR Foot Sensor Board  
Look closely at the soles of your Bioloid’s feet.  Those little round indentations were clearly designed to accept 0.2" FSR’s.  This interface board can read 4 FSR’s, enough for one foot.  The board fits neatly into the foot, and plugs into the Dynamixel network.  The kit includes the board, 4 FSR’s, and leads for the sensors.

If you have any questions, or you need advice about using these boards, go ahead and post about it in the TRC Forums.

PhidgetStepper USB Stepper Motor Controller

Wednesday, April 30th, 2008

We have some exciting news for all of you fine people who have been calling us up over the years asking why there isn't an inexpensive plug-and-play solution for controlling stepper motors from a computer.  Phidgets has just released the PhidgetStepper Unipolar 4-Motor controller!  This little board, which is retailing for just $72.74, allows you to control up to 4 unipolar stepper motors from your USB port.  Building a CNC rig?  Building a wheeled robot that will need fast, precise speed and position control?  Buy this controller.

From the official press release:

 

Phidgets adds a $75.00 stepper controller to its line of motor controllers

The 1062 – PhidgetStepper Unipolar 4-motor, can control up to 4 stepper motors.

CALGARY, Alberta, April 29, 2008 ― Phidgets Inc. today announced the addition of a new product to its family of motor controllers. The 1062 Stepper controller controls the position, velocity and acceleration of up to 4 unipolar stepper motors. Applications that require precise
positioning are well suited for this device. The stepper controller can also run the motor in continuous rotation mode by giving it a large position address. Using the upper position limit as an address would, for example, rotate the motor for 45 years.

The 1062 plugs directly into the computer’s USB port and comes with a USB cable. Like all Phidgets, application programs can be written using the Phidgets API. “The 1062 Product Manual’s Technical Section contains valuable information and programming tips on how to
use the API functions to drive stepper motors,” said Bernard Rousseau, Phidgets Director of Marketing. “We continuously update our documentation in an effort to make it as easy as possible for our users to get their projects going”, added Rousseau.

“We already offer Servo controllers, and a variety of DC motor controllers. The arrival of a stepper controller fills a void in our family of motor controllers. ” says Chester Fitchett, CEO of Phidgets. “We have paid close attention to costs in order to give our customers the value/price ratio they are expecting from Phidgets.” added Fitchett.

Product Specifications
Position Resolution: ½ step (40-bit signed)
Upper Position Limit: 239 – 1 ½ steps
Lower Position Limit: -(239 - 1) ½ steps
Velocity Resolution: 0.75 ½ steps/second (9-bit)
Velocity Limit: 383.25 ½ steps/second
Acceleration Resolution: 140.625 ½ steps/second2 (6-bit)
Acceleration Limit: 8859.375 ½ steps/second2
Minimum Power Supply Voltage: 5V
Maximum Power Supply Voltage: 12V
Max Current Per Coil: 1A
USB-Power Current Specification: 100mA max
Device Quiescent Current Consumption: 23mA
Device Active Current Consumption: 23mA max
Software Environment

“Unlike a lot of our competitor’s products that require their users to write some firmware code in order to use their sensor, we are completely “Plug and Play” says Bernard Rousseau, Director of Marketing. “With Phidgets, you plug it in and start using it and when it comes to programming, the user, not us, decides which operating system and which computer language he wants to use”, added Rousseau.

Users can program Phidgets using a simple yet powerful and well documented Application Programming Interfade (API) that is supported under Windows (2000, XP, Vista), Windows CE, Mac OS X, and Linux. Users can write programs in Visual Basic, VB.NET, C#, C/C++, Flash/Flex, Java, Labview, Matlab, ActionScript 3.0, and Cocoa.

Phidgets also provides programming examples for all its products to help programmers write their own programs. The API Libraries as well as the examples and the documentation are available at no charge on www.Phidgets.com.

New Products: Hitec R/C, Cool Sensors, and More!

Monday, April 28th, 2008

 

Hitec Laser 6 FM 75MHz Radio System

We now sell Hitec’s Laser 6 RC Tx/Rx set.  This is the first standard R/C control set to be added to our catalog, and it’s about time.  We know that not everybody needs or wants to build autonomous robots, and we’re cool with that.  The kit includes the 6-channel Laser 6 transmitter, HFD-08RD 8-channel receiver, and two HS-322 servos.  This set offers a great solution for no hassle, plug-and-play control of servos and DC motor controllers.

The Robonova 1 humanoid can easily be adapted to work with this controller, too.  RC inputs on the Robonova are interpreted as analog values, which can be used to trigger and alter motion sequences in a wide variety of ways.  Fun stuff!

 
SoftPot Linear Membrane Potentiometer - 100mm

These touch-sensitive linear potentiometers are really cool.  The resistance varies linearly depending on where pressure is applied to the sensor.  The pinout is just like any other 3-pin potentiometer, and the pins have a breadboard-friendly pitch of 0.1", so integrating it into your project is a snap.

 
 
Resistive Flex Sensor 4.5"

These resistive flex sensors are made of one resistive element, which varies from 9 kOhm when straight to 22 kOhm when flexed 180 degrees.  You can use them for monitoring joint angles, as electronic "whiskers," or any other application that calls for a simple, inexpensive flex feedback.

 
 
PIR Motion Sensor

For a while now, we’ve been looking for a cheap, simple motion sensor to satisfy the needs of our home automation customers.  Well, it looks like we’ve found it.  This little sensor is about 1" wide, only consumes a few milliamps, and presents a simple digital output.  The sensor outputs 5V when there is no motion, then when it senses something, the output drops to zero.

 
Arduino Serial USB Adapter Board

This breadboard-friendly adapter converts USB to TTL-level serial, appearing as a virtual COM port on your computer.  It was designed for programming and communicating with the Arduino Stamp, but it also works as a generic serial interface.

 
Sparkfun Jumper Wires F/F (Set of 10)

Do you need to connect some pins to some other pins?  Well, then you need some female-to-female jumpers.  They’re good for wiring up sensors whose pinouts don’t match the connections on your microcontroller or interface board.

 

Now, go buy some stuff, build something cool, then tell us all about it in the forums!

You may have noticed that the bulk of the products in this update are SparkFun products.  They’re really cool people to work with, they produce and procure a ton of cool and useful stuff, and we keep adding more of it to our catalog, in our quest to bring you the finest products all under one roof.  To see all of the SparkFun products that we sell, follow this link to our SparkFun category.

UPDATE: You can also, any time you want, see the 27 most recent products to be added to our catalog.  Bookmark it.  You know you want to.

Laser Harp Mk. III: Now With More Wiimote

Friday, April 25th, 2008

Stephen Hobley is at it again.  His laser harp was cool enough to win second place in our project contest a few months back, and since then he’s managed to make it even cooler.  Using a Wiimote to accurately track the positions at which the beams are interrupted, he added some very clean and precise pitch control to the already impressive instrument.  Watch the video.  After about a minute of demonstration, he gives a quick explanation of how the modification works, so be sure to watch the whole video.

He started a thread about this in our forums, so head on over there to give him props, ask questions, etc:
Laser Harp Mk III

If you haven’t read the original thread from when he first completed the project, check it out here:
Frameless Laser Harp

If you want more info on how it was made, or if you want to build your own, follow this link to Stephens’s site:
The Laboratory

New Wireless Products: GPS & Bluetooth

Friday, April 18th, 2008

We've been adding new products to the catalog like crazy lately, so we figured now would be a good time to make sure you knew about some of them.  To start you off, here’s a cool way to add GPS to computer-controlled robot:

Lassen iQ GPS Receiver

This is a USB-interfaced GPS receiver.  The kit includes a Trimble Lassen IQ Receiver, an interface board created by SparkFun, and everything else you need to tap into the GPS network.

And here are some Bluetooth modules so you can get rid of all those wires and tethers you keep tripping over:

Parallax EmbeddedBlue Transceiver AppMod

This Bluetooth module from Parallax was designed for easy integration into any Basic Stamp 2 project.  It works great with the Board of Educationn, BOE Bot, or SumoBot mini sumo robot.  We also offer the Microsoft Robotics Studio-compatible BOE Bot kit, which includes the EmbeddedBlue module.

 
BlueSMiRF Silver

The BlueSMiRF is a very simple to use Bluetooth modem.  It acts as a serial bridge, and it’s practically a drop-in replacement for any wired connection.  Works great with any microcontroller system, including Arduino and Basic Stamp.

 
RooTooth

This little jobber is a Bluetooth Wireless adapter for the iRobot Roomba robotic vacuum.  Use it to control your Roomba from your computer, cell phone, PDA, or whatever Bluetooth device you happen to be using.  Chase your pets, stage Roomba sumo matches, set up synchronized Roomba dance routines… Or you could just vacuum the floor.  Whatever floats your boat, man.

 
Bluetooth USB Module

A simple, cheapo USB Bluetooth adapter.  There isn’t much more that needs to be said.  Use it to connect your computer to all of your other Bluetooth gizmos.

 

That’s all for now.  Stay tuned for another big update next week!

Announcement: Trossen Robotics Community Chat Rooms

Monday, April 14th, 2008

Greetings!

After much anticipation (and a few stumbling blocks) we’re happy to officially announce, the Trossen Robotics Community (TRC) Chat Rooms! The TRC is currently in the process of deciding which night(s) are the best for everyone to have some discussions on everything robots. To join in and cast your vote, log into your TRC account and check out this thread. We will continue to move these chatrooms forward, including adding more rooms, setting up topics for discussions, etc.. So get in there and start chatting!

To get your botchat on, simply log into your TRC account and click the TRC Chat image in the left column:

trc screenshot

This module contains all of the stats on the chat rooms and is available on all pages in the TRC:)

We hope you enjoy this new feature, because there are a lot more great features to come in the TRC!

Announcement: Trossen Robotics Community Contest Prize

Monday, April 14th, 2008

After the incredible projects and hard time we had deciding on the winners, we needed a quick cool down from the last Trossen Robotics Community (TRC) contest!

However, we are now ready to announce the prizes and dates for this round in the TRC Contest. We’ve decided to do something a little different for this round; instead of offering cold hard cash, we’re going to be offering what else? Robots!! Yes, act soon and if you get your project in before July 31th 2008, you can win your very own Robot:)

Ok, all cheesiness aside, here are the prizes for this round’s TRC Contest:


1st place

Crustcrawler SG5 Robot Arm

Includes:

2nd place

(Open Link in IE to view site)


Silverlit R/C X-UFO

Features:

  • Gyro stabilized
  • Indoor and outdoor
  • All factory assembled
  • Unique electronic control system
  • Ultra lightweight carbon fiber frame include 2-way charger-AC adapter or
    automotive adapter
3rd place

Wowwee Alive™ - ELVIS®

Modes:

  • Alive (Taking care of business™) mode
  • Song mode
  • Monologue mode
  • Sing through (Share the spotlight) mode

As always, for contest details and qualifications please visit our contest page.

Hexapods show off writing skills

Wednesday, April 2nd, 2008

We’ve had some very cool multi-legged walkers showing up in our forums and blog in the past few months, including Kåre Halvorsen’s Phoenix and Matt Denton’s B.F.Hexapod, and we’ve been really impressed by the varying capabilities and gait calculation methods they’ve used.  Taking it to the next level, the builders have decided that they’re not content with just making their robots walk about and wave their legs around any more.  In February, Phoenix learned a new trick:

Then Denton gave it a shot with his B.F.Hexapod, showing off some impressive drawing skills:

If you want to see more info, or to drill these guys for more information on their projects, hit up the forums.  Kåre’s thread; Matt’s thread.

Get your Bot Mag back issues right here!

Tuesday, March 25th, 2008

We now have the full run of Robot Magazine back issues available in our catalog, for just $5.99 per issue.  That’s almost three years of robot goodness!  Every issue is packed with product reviews, robot building tips, industry insights, and more.  Visit our Robot Magazine back issue section for more information about each issue, as well as links to free online content.

I can only assume that, having seen this, you’re about to go order all of the back issues so you can catch up on all the cool news you’ve been missing.  Go do that, and then head over to BotMag.com and subscribe!

Trossen Robotics Garage Sale!

Tuesday, March 18th, 2008

It's spring cleaning time, folks!  We're clearing out some of our storage space to make room for new stuff, so we're offering up some great kits for dirt cheap.  Here are some recent additions to the Trossen Robotics Garage Sale:

Superdroid Tri-Wheel Omni-Directional Vectoring Robot Kit

Vectoring omni-directional bots are really cool, and you know you've always wanted one.  Buy this kit, give it a brain, and then come post about it in our forums.  The platform is 12" on each side, so there's plenty of room for a small single-board computer.

Included: All the nuts and bolts, 2 platforms, battery packs, dual-layer omni-wheels, hubs, motors, and wires.  Basically a complete hardware package.  All it needs is motor controllers, a brain, and… you.

Sale Price: $200

 
24V 3.6Ah NiMH Intercooled battery pack

The cells are spaced for air flow, and and the pack is equipped with two built-in fans.  Active cooling allows for longer high-current operation and faster charging.

Sale Price: $40

 
BattleKits Feather Weight Kit

16 inches wide by 16 inches long, this is the baby of the BattleKits family.  Despite (or perhaps because of) it's small size and simple design, this is a bad ass battle bot platform.  It has great mobility thanks to its two 3-horsepower 24V motors, and the slotted top panel allows the wheels to be in contact with the ground even if the bot gets flipped.

Included: Chassis, motors, wheels, battery pack, Ampflow Mini motor controller… all you need is an R/C receiver or other control signal source, and of course some flame throwers and pneumatic rams and spinning blades and whatnot.

Sale Price: $700

 
BattleKits Light Weight Kit

16 inches by 18 inches, four wheel drive.  Chassis only.  No motors, batteries, or controller.

Included: Chassis, wheels, and drive mechanism.

Sale Price: $400

 
BattleKits Middle Weight Kit

21 inches by 22 inches, four wheel drive.  Comes with two S28-400 dc motors, each churning out a hefty 4.5 horsepower.  The motors themselves are worth the price of this kit.

Included: Chassis, wheels, drive mechanism, motors.

Sale Price: $600

 
BattleKits Heavy Weight Kit

This is the granddaddy of the BattleKits line.  The chassis itself (which, coincidentally enough, is all we're selling here) is 30 inches by 24 inches and weighs 87 lbs.  This thing is solid as a rock.

Included: Chassis, wheels, and drive mechanism.

Sale Price: $500

 
BattleKits Drive Modules
Module A, Module B

Don't want a whole BattleKits chassis?  Bolt these onto your own design.  We only have one of each (form A and form B) left in stock, so it's perfect if you only need two wheels.  Motors not included.

Included: Chassis, wheels, and drive mechanism.

Sale Price: $80 per module

 

That’s it for now, but keep your eye on the Garage Sale.  You never know what you’ll find.