Cart/Login/Help Tutorials Blog Community Contact
Become an Affiliate!

Archive for the ‘Flying Robots’ Category

WowWee FlyTech Bat Unboxing

Tuesday, June 10th, 2008

Our friends over at RoboCommunity have just sent us a link to an unboxing thread of the WowWee FlyTech Bat:

FlyTech Bat

Designed to totally creep the living hell out of you at the same time that you’re terrorizing your dog/cat/iguana/Geico Gecko, this bat flies vertically, yes vertically in the air! What really impressed me was the charge vs. operating time being near equal. It took a mere 4 minutes in order to get between 5-7 operating time! Hey, considering these large humanoids getting like an hour or so tops for a 4-5 hour charge, this is really impressive!

What in the world is FlyTech you ask? FlyTech is a new series of really cool toy robots from WowWee. Yes, they all fly, and do a pretty good job at it too! You can check out all of the exciting new robots at FlyTech Online or over in RoboCommunity’s FlyTech Category.

via RoboCommunity

Surveyor SRV-UAV?

Tuesday, December 4th, 2007

Ok, this is just too damn cool. The Surveyor crew have integrated the SRV-1 controller with a quad-rotor helicopter.

The heli, called "X-3D-BL Scientific," is from a German company called Ascending Technologies GmbH.  I knew it was easy to use the SRV-1 controller for other wheeled vehicles, but seeing it on a UAV is pretty exciting.  They don’t have too much info up yet, but it sounds promising.  Here’s a video of the aircraft (without SRV-1 controller) in action:

Check out the original post, and keep an eye on the Surveyor Robotics Journal for updates!

The Wowwee Dragonfly is Here !

Thursday, August 23rd, 2007

When the new Dragonfly came in we charged one up and ran downstairs to try it out right away. We started out in the lobby and it took about 45 seconds for us to get yelled at (never lease to robot geeks) so we took it outside.

It took us a few minutes to figure out how to fly it. Here are the things we learned: The main thing to remember is to not try to throw it when launching it. It works best when you just let it go with a really gentle forward motion. It also will fly best in no wind environments, due to it being so light. It also needs a decent amount of room to get around so I really wouldn’t plan on flying this indoors too much.

The Dragonfly really is a lot of fun. It’s uncanny how fast you forget it’s an RC toy and feel like it’s a really a large insect flying around in front of you. The flapping wings and shape of this toy really seem to trick the mind in to thinking it’s seeing a real live animal.

We were surprised how well this product worked for under $50. You really can steer it around. For a foam toy it’s pretty crash resilient. We did break one wing, but after that we crashed it plenty of times with no problems. (It comes with a set of spare wings.) The battery life was also impressively long. We expected it to be really short like the PicoZ, but it lasted at least twice as long if not more. This is a great toy to play with in the yard or at picnics. The Dragonfly is a good gift idea. We don’t recommend it for young kids however, quick eye hand coordination is needed to fly it.

Project CONDOR: Musical dirigibles descend on Chicago!

Friday, June 29th, 2007

Let’s get right to the heart of this thing.  Project CONDOR is a high-tech immersive multimedia sensory experience.  An array of eight robotically controlled helium-filled blimps, each with a speaker hanging from it, dynamically repositioning sound sources, with audio streaming to each blimp via Bluetooth, playing a separate part of an electronic musical composition, floating around inside a large indoor space, accompanied by a light show and video projections…  I’m on the verge of a flashback just from writing that sentence, so I can only imagine how trippy the actual performance is going to be.  Tonight and tomorrow night (That’s June 29 and 30, 2007), starting at 8 pm, Project CONDOR will take flight in Chicago’s Broadway Armory.  Admission is only 10 bucks, and I have no idea how many people they’re letting in, so get there early if you want to check it out.

Thanks to Chicago Public Radio for covering this story while I was on my way to work this morning.  Their pledge drive is still going on, so head over to WBEZ.org and give them some money.

Story at news.big.net

Project CONDOR event posting at Metromix

psychedelic blimp!
I couldn’t find any Project CONDOR pictures, so I ran a Google image search for “psychedelic blimps” and this is what I got.

Coandă Effect Flying Saucer

Tuesday, April 3rd, 2007

N02a

N02

N02

N02

This army project has been making the rounds on the internet. The Flying Saucer works using the Coanda Effect which makes for a compact blade system to lift a larger bodied object. Pretty smart!

Related Links:
Wired - most in depth info
JNL Labs - Pictures of Assembly
Coandă effect @ Wikipedia

Draganflyer Gyro Stabilized RC Helicopter

Tuesday, February 27th, 2007
Draganflyer

Anyone looking into building serious flying robots should take a look at the Draganflyer line from Draganfly Innovations. These are some high quality flyers for very decent prices. Info about the Draganflyer from their website:

Draganflyer SAVS Stabilized Aerial Video System Gyro Stabilized RC Helicopter

The Draganflyer r/c helicopter just got better; with the new Draganflyer Stabilized Aerial Video System (SAVS) it has never been easier or more economical to create superior, professional quality, aerial video. The SAVS takes up the slack where full size aircraft fall short, low level and close up video. For everything from real estate to surveillance or music videos the SAVS will excel with its high resolution CCD wireless video camera and anti-vibration mounting system. The complete Draganflyer SAVS comes pre-assembled with a wireless video camera system, transmitter, batteries and charger all packaged in two compact, custom built hard-shell cases. Built on the tested and proven Draganflyer V Ti platform and equipped with a high resolution CCD video camera and numerous state of the art features the Draganflyer SAVS is one of the most high-tech aerial video system in the world.

Link with videos after the jump

check out their entire helicopter line hereÂ