Javascript Menu by Deluxe-Menu.com
 

Archive for the ‘DARPA’ Category

Dean Kamen and the Robotic Arm

Thursday, May 17th, 2007

Ok, we’ve seen some pretty incredible advancements in robotics these last couple of years, but this tops the cake! The articulation from this arm is amazing. It looks like something straight out of the Cyberdyne lab in the Terminator series.

via (BoingBoing)

BOSS - GM’s DARPA Grand Challenge Entry Unveiled

Monday, April 16th, 2007

GM has unveiled an entry into the Defense Advanced Research Projects Agency (DARPA) Grand Challenge competition on November 3, 2007. For those that have been living in a cave and haven’t heard of the DARPA challenge yet, from the Grand Challenge website, “The Urban Challenge features autonomous ground vehicles maneuvering in a mock city environment, executing simulated military supply missions while merging into moving traffic, navigating traffic circles, negotiating busy intersections, and avoiding obstacles”.

Neither of the past DARPA competitions (2004, 2005) attracted much interest from the automotive industry, mostly because creating an autonomous vehicle to travel across the types of roads and other conditions that past competitors were exposed to simply didn’t fit into their business model.

DARPA Boss

It’s sad but at the same time exciting to hear that corporations are starting to participate in this autonomous vehicle competition. I’d much rather see the past methods continue of corporate sponsorship of teams rather than the actual corporation itself participating, but hey; If this is what has to happen in order for us to see these robotic vehicles on the road and taking ourselves to and from work everyday without us having to touch the wheel then so be it. I’d love to see the day when my car drives itself and I can catch up on things that I need to do while I’m on my way to/from work.

Inside of Boss

Named “Boss” for Charles “Boss” Kettering, this Tahoe has over 25 external sensors, the computing power of ten Compaq Intel Core 2 Duo laptops, and many other electric and electronic devices all powered by an auxiliary 8-kW generator under the hood.

via (Robot Stock News, Motor Trend)

Team Lux readies Volkswagen Passat TDI for DARPA Urban Challenge

Thursday, March 22nd, 2007
Engadget Lux image

“Although a fair amount of entrants into DARPA’s Urban Challenge flank their vehicles with hordes of less-than-attractive sensors, we’ve been quick to forgive such atrociousness due to the complexities involved in cruising around sans a driver. Ibeo-led Team LUX, however, is looking to add a dash of style to this year’s (now lucrative) competition, as its Volkswagen Passat TDI wagon touts a clean exterior, three “laser scanners” for complete 360-degree perception, and amazingly, not much else. Apparently, the trio of uber-capable modules are all that’s needed to keep the car under control, and while we’d typically doubt such bold claims, the 11-member team has quite an impressive resume in the autonomous vehicle department. Still, the minimalist approach will probably face some stiff competition, and although we’re certainly not experts on design, we still think the Wolfpack’s Lotus packs a bit more sexy.
via (Engadget)

Under the hood of Stanford’s robotic race car

Wednesday, February 21st, 2007
Stanford-robotic-race-car

A view of the “brains” of “Junior,” a modified 2006 Volkswagen Passat wagon being developed by Stanford University’s Racing Team to compete in DARPA’s Urban Challenge in November. The competition among driverless cars will take place on city streets, among other cars.

Read Article

via Digg post

Darpa wants Luke’s replacement hand from Star Wars

Wednesday, February 21st, 2007
robotics limb

Thought-controlled robotic limbs were only the beginning.

hand.jpgScientists have had a string of remarkable successes lately, taking signals from the brains of monkeys and men, and using them to move mechanical arms.

Darpa, the Pentagon’s blue-sky research division, now wants to ratchet that work up about ten notches, by developing a “neurally controlled artificial limb that will restore full motor and sensory capability to upper extremity amputee patients. This revolutionary prosthesis will be controlled, feel, look and perform like the native limb.”

read more

via Digg

OpenCV - Open Source Computer Vision Library

Thursday, February 15th, 2007

Thanks to the hard work of 20 developers, there is an open source vision library, freely available to the public, named OpenCV.

This library is mainly aimed at real time computer vision. Some example areas would be Human-Computer Interaction (HCI); Object Identification, Segmentation and Recognition; Face Recognition; Gesture Recognition; Motion Tracking, Ego Motion, Motion Understanding; Structure From Motion (SFM); and Mobile Robotics.

Wondering about some credentials and how well this software works? OpenCV was used as the vision system of “Stanley”, the winning entry to the $2M DARPA Grand Challenge race of 2005.

Yahoo Group Stanley

Wondering what kind of a support community is out there for a vision library of such a caliber? There is a Yahoo Tech Group currently with 23,804 members who are contributing to this library’s success. If your interested in being a part of this community, join this group and find more out about this library and what you need to do to get started with implementing it in your own projects.

Convinced? I thought so. The library can be downloaded at the OpenCV Sourceforge Page, where more information can be found about the library as well.

via Intel

NOVA program on the DARPA Grand Challenge available online

Monday, January 22nd, 2007
darpaonline

If you happen to have missed the NOVA hour long documentary on the DARPA grand challenge you can now watch it from their website. This is why we love the internet.

Link

UAVs are Coming and We Want One!

Wednesday, December 20th, 2006
SoldierTech_WASP

THIS IS NOT A TOY: Micro Air Vehicle Weighs Less, Flies Longer

About as long as a No. 2 pencil and as heavy as a cellphone, the Wasp may look like a toy, but this tiny Micro Air Vehicle (MAV) has broken records with a flight time of 1.5 hours and can fly like a helicopter — just don’t point it at your sister or the family pet.

Read More

UAV

Mini Helicopter Thinks for Itself — On the Fly — to React to Dangerous Situations — Now Transitioning to Military

Unmanned aerial vehicles (UAVs) are one step closer to someday matching — and possibly surpassing — their human-piloted counterparts, thanks to the completion of a project successfully tested by Georgia Tech and sponsored by the Defense Advanced Research Projects Agency (DARPA) and the U.S. Air Force Research Laboratory. The project was supported by DARPA’s Information Exploitation Office with Dr. John Bay serving as the program manager.

Read More

No Prize Money for DARPA 2007?

Friday, October 20th, 2006

After Stanford University won a Pentagon robot race through the Mojave Desert last year, engineers and students hoisted an oversized $2 million check and poured bubbly champagne over their unmanned Volkswagen SUV.

Next year’s winners won’t be as rich.

The Pentagon’s research arm, which has twice hosted the high-tech contests since 2004, blames an obscure section in a defense spending law signed by President Bush this week. The Defense Advanced Research Projects Agency believes the law prevents the agency from awarding the $2.7 million prize money.

So instead, DARPA will hand out shiny trophies to the top three teams whose smart vehicles can weave through congested city traffic without human help.

“I promise that the trophies will be given because I’ll personally buy them myself,” Tony Tether, DARPA’s director, told competitors earlier this year.


Read the full article here