Cart/Login/Help Tutorials Blog Community Contact
Become an Affiliate!

PhidgetStepper USB Stepper Motor Controller

April 30th, 2008 by Dave

We have some exciting news for all of you fine people who have been calling us up over the years asking why there isn't an inexpensive plug-and-play solution for controlling stepper motors from a computer.  Phidgets has just released the PhidgetStepper Unipolar 4-Motor controller!  This little board, which is retailing for just $72.74, allows you to control up to 4 unipolar stepper motors from your USB port.  Building a CNC rig?  Building a wheeled robot that will need fast, precise speed and position control?  Buy this controller.

From the official press release:

 

Phidgets adds a $75.00 stepper controller to its line of motor controllers

The 1062 – PhidgetStepper Unipolar 4-motor, can control up to 4 stepper motors.

CALGARY, Alberta, April 29, 2008 ― Phidgets Inc. today announced the addition of a new product to its family of motor controllers. The 1062 Stepper controller controls the position, velocity and acceleration of up to 4 unipolar stepper motors. Applications that require precise
positioning are well suited for this device. The stepper controller can also run the motor in continuous rotation mode by giving it a large position address. Using the upper position limit as an address would, for example, rotate the motor for 45 years.

The 1062 plugs directly into the computer’s USB port and comes with a USB cable. Like all Phidgets, application programs can be written using the Phidgets API. “The 1062 Product Manual’s Technical Section contains valuable information and programming tips on how to
use the API functions to drive stepper motors,” said Bernard Rousseau, Phidgets Director of Marketing. “We continuously update our documentation in an effort to make it as easy as possible for our users to get their projects going”, added Rousseau.

“We already offer Servo controllers, and a variety of DC motor controllers. The arrival of a stepper controller fills a void in our family of motor controllers. ” says Chester Fitchett, CEO of Phidgets. “We have paid close attention to costs in order to give our customers the value/price ratio they are expecting from Phidgets.” added Fitchett.

Product Specifications
Position Resolution: ½ step (40-bit signed)
Upper Position Limit: 239 – 1 ½ steps
Lower Position Limit: -(239 - 1) ½ steps
Velocity Resolution: 0.75 ½ steps/second (9-bit)
Velocity Limit: 383.25 ½ steps/second
Acceleration Resolution: 140.625 ½ steps/second2 (6-bit)
Acceleration Limit: 8859.375 ½ steps/second2
Minimum Power Supply Voltage: 5V
Maximum Power Supply Voltage: 12V
Max Current Per Coil: 1A
USB-Power Current Specification: 100mA max
Device Quiescent Current Consumption: 23mA
Device Active Current Consumption: 23mA max
Software Environment

“Unlike a lot of our competitor’s products that require their users to write some firmware code in order to use their sensor, we are completely “Plug and Play” says Bernard Rousseau, Director of Marketing. “With Phidgets, you plug it in and start using it and when it comes to programming, the user, not us, decides which operating system and which computer language he wants to use”, added Rousseau.

Users can program Phidgets using a simple yet powerful and well documented Application Programming Interfade (API) that is supported under Windows (2000, XP, Vista), Windows CE, Mac OS X, and Linux. Users can write programs in Visual Basic, VB.NET, C#, C/C++, Flash/Flex, Java, Labview, Matlab, ActionScript 3.0, and Cocoa.

Phidgets also provides programming examples for all its products to help programmers write their own programs. The API Libraries as well as the examples and the documentation are available at no charge on www.Phidgets.com.

Share and Enjoy: These icons link to social bookmarking sites where readers can share and discover new web pages.
  • Digg
  • del.icio.us
  • Netvouz
  • DZone
  • ThisNext
  • MisterWong
  • Wists
  • Google
  • Live
  • NewsVine
  • Reddit
  • Slashdot
  • SphereIt
  • StumbleUpon

Tags: ,

One Response to “PhidgetStepper USB Stepper Motor Controller”

  1. [M]etabrain [E]ntry [L]og » Blog Archive » Presentations at the Media Lab today Says:

    […] sent the robotics mailing list at Olin a heads-up on some nifty toys. Nothing earth-shattering (okay, the ability to rapid-prototype stepper motors in a […]

Leave a Reply