Cart/Login/Help Tutorials Blog Community Contact
Become an Affiliate!

NEW AND IMPROVED Surveyor SRV-1 webcam rover

December 4th, 2007 by Dave

The immensely popular Surveyor SRV-1 has just received some major upgrades!  The tracked base remains unchanged, but the electronics have gotten a complete overhaul.  Wi-Fi has replaced the slow and sometimes unreliable ZigBee wireless link, the camera can now grab video at a maximum resolution of 1280 x 1024, an Analog Devices Blackfin processor has replaced the comparatively puny ARM7 processor, and they've even added laser pointers for distance sensing.

Wi-Fi:

The SRV-1 now benefits from the extended range and faster data rates of Wi-Fi.  All you need is an 802.11 b/g wireless LAN card and you're ready to start spying on the neighbors.

Camera:

Speaking of spying on your neighbors, this 1.3 Megapixel camera is roughly on par with most cell phone cameras, with a maximum resolution of 1280 x 1024.  Unlike your cell phone camera, this one’s going to be riding on tank treads.

Main Processor:

Here it is, fully assembled.  The red board on top carries the 1000MIPS 500MHz Analog Devices Blackfin BF537 processor.  [Editor’s note: When I was 17, I built my first computer around the 500MHz Pentium, which was the top of the line at the time.  Now you can get all that power on a circuit board that’s smaller than a playing card.  Crazy, huh?]

Lasers:

Fact: lasers make anything cooler.  The new SRV-1 uses two parallel lasers as a low-cost range-finding system.  Try not to blind your friends/family members/pets.

Links:

Purchase the new and improved SRV-1

More information (Manufacturer’s site)

Share and Enjoy: These icons link to social bookmarking sites where readers can share and discover new web pages.
  • Digg
  • del.icio.us
  • Netvouz
  • DZone
  • ThisNext
  • MisterWong
  • Wists
  • Google
  • Live
  • NewsVine
  • Reddit
  • Slashdot
  • SphereIt
  • StumbleUpon

Leave a Reply