Cart/Login/Help Tutorials Blog Community Contact
Become an Affiliate!

iRobot Create Challenge: Entry Compilation

June 27th, 2007 by Alex

For those of you that do not know, the iRobot Create Challenge is just that, a challenge to see who comes up with the most creative idea with the fully programmable iRobot Create Platform! Well, Don over at Tom’s Hardware has put together a nice compilation of the publicly available entries into the challenge.

This one was by far my favorite:

IRobot Tennis

Taken from the post:

Professor David P. Miller of the University of Oklahoma has managed to program the iRobot Create to see and respond to visual stimulus. Using an XBC robot controller - complete with camera and firmware that allows the robot to track multiple objects of different colors - Professor Miller has gotten the iRobot Create to play tennis. It tracks a colored ball to its side of the net and returns it at an angle that the robot calculates as appropriate. To clarify, this robotic “tennis” is a bit slower than human tennis but the mechanics are there. It’s impressive, and you can find movies of this project and others at Adding vision to the iRobot Create

Read the full post

Share and Enjoy: These icons link to social bookmarking sites where readers can share and discover new web pages.
  • Digg
  • del.icio.us
  • Netvouz
  • DZone
  • ThisNext
  • MisterWong
  • Wists
  • Google
  • Live
  • NewsVine
  • Reddit
  • Slashdot
  • SphereIt
  • StumbleUpon

Leave a Reply