A new KHR-series Kondo humanoid robot is coming out… and we’ll be carrying it!
November 29th, 2006 by AlexKondo has yet another humanoid biped robot to add to their product line called the Kondo KHR-1HV.
Oddly enough, the name has a lower version number than the previous version of the KHR series robot, the KHR-2HV. That aside, this new version sports 19 degrees of freedom, which enables the humanoid to rotate each leg independently at the hip. Additionally, each shoulder in the KHR-1HV are now equipped with KRS-4024SHV servos which are metal geared, and have greater range of rotation. Of course, all of these upgrades come with a cost; Estimated at 126,000 yen (about $1,091 US).
It looks like this robot has quite a bit more potential than the 2HV. I can just see it now… Kondo Martial Art Competitions!!
Thanks to our friends at Robot Dreams for finding this lead!
UPDATE: We are now carrying this Kondo 1HV!!