Archive for the ‘News / Articles’ Category

Boston Dynamics does it again

Monday, October 26th, 2009

Whoa. Just Whoa.

I won’t even pretend that I understand all that is going on in the walking gait here, but this is darn near human-like in every aspect. And being able to walk like that is one thing, being able to recover from a sideways push is an entirely different accomplishment all together. Absolutely brilliant.

One Step Closer to T-1000!

Thursday, October 15th, 2009

Looks like iRobot is determined to bring Judgment Day upon us. First with the military bots, and now they’re trying to build a liquid-metal-shape-shifting robot that will surely ask us if we are John or Sarah Connor. Okay, not quite, but it looks like they’re headed in that direction.

This week at IROS 09 (Intelligent Robots and Systems), iRobot and the University of Chicago unveiled a soft, blobby robot that looks something like an inflating marshmallow.

The new robot, called chembot, changes the shape of its stretchy polymer skin using a technique called “jamming skin enabled locomotion”. This means that different sections of the robot inflate or deflate separately; controlling this inflation and deflation enables the robot to move. DARPA, which is funding the project, hopes to use the robot to squeeze into small holes or under doors, which I’m guessing would be used for sophisticated surveillance.

Via Geekology

Matt Trossen, Hagetaka, and Roboard Featured in Make Magazine

Monday, September 21st, 2009

This month’s Make Magazine (Issue 19) is the yearly Robotics Hobbyist special, and features my boss Matt Trossen once again stealing all of my glory and talking about his take on the current state of hobby robotics. That is okay however, and I’m prepared to take it with stride because anyone reading this blog knows I’m the true brains behind this operation. Not only that, but I’m also better looking (it’s the beard) and I embrace an air of dignity and modesty.

Speaking of my dashing good looks and superior mental prowess; Make also featured my currently shelved and ego-crippling project Hagetaka. Rest assured; my wife and 2 year old have picked up 2nd jobs to fund this project further and it will return with even stronger servos and bigger guns, ready to assist me in my plan for world domin- err, winning Mech Warfare.

Last but not least, Make Magazine readers got a quick and to the point review of the Roboard, the first full featured Robotics Computer on the market.

But seriously, be sure to pick up a copy as the entire issue is full of fun projects and robotic tidbits sure to appeal to your average robot-geek. And like Christmas, it only comes once a year!

m19cover

Can You Smell What Lynxmotion Is Cooking?

Friday, September 11th, 2009

Our good friends over at Lynxmotion have been a force to be reckoned with for well over a decade in the robotics industry; producing some truly inspiring and amazing robots over the years. My first ‘real’ robot was a Lynxmotion Hexapod 1 (the 3 servo variety) that I picked up back in 1997, and their product lines were one of the driving forces that got me addicted to robotics.

hunchie7

Well, they’ve impressed me yet again; Lynxmotion owner Jim and his son James, being robot enthusiasts and likewise fans of the Mechwarrior franchise, were intrigued with the Mech Warfare competition. Specifically they loved the biped aspect of it and so they set out to create a low cost competitive platform for Mech Warfare, and succeeded. Nicknamed ‘Hunchback’ and based around their BRAT biped platform, this is turning out to be one of the lowest cost and straight forward platforms for the competition. Currently there is a work-in-progress tutorial showing the build and code, and it looks like we have a very high chance of being treated to a complete kit allowing you to build your very own. If you’re interested in seeing how it progressed from prototype to near final revision, check out the project thread over on the Lynxmotion forums. Check out the following video of the Hunchback in action!

arbotiX – Advanced Robocontroller for the Bioloid System

Thursday, September 3rd, 2009

We’re good friends with the folks over at Vanadium Labs; some very talented people who have been in the robotics game for quite awhile but have just now established their official company. This is great news for the robotics community however, as they have some pretty amazing products on the horizon. One product in particular is the new arbotiX Robocontroller, an advanced Open Source microcontroller tailored for the Bioloid system and AX-12+ servos.
arbotix

The arbotiX robocontroller is an advanced control solution for small-to-medium size robots. It incorporates a powerful AVR microcontroller, XBEE wireless radio, dual motor drivers, and 3-pin servo-style headers for IO.

The arbotiX robocontroller is specifically designed to control robots built using Bioloid servos, although it is also a very high-end solution for powerful rovers. It is not intended to be a drop-in replacement for a CM-5, rather it is intended as a high level development tool for building more sophisticated robots.

So what we have here is an Arduino IDE compatible microcontroller with a plethora of I/O, plug and play capable with AX-12 servos, and an Xbee Wireless Link to your PC. It’s also worth mentioning that this was the controller used in the robot that won Year 1 of Mech Warfare, Issydunyet. For more information on the controller check out the Vanadium Labs website.

Trossen Robotics will be exclusively distributing this exciting and powerful new Robocontroller with an estimated release date of Mid-October 2009. We’ll have more details in the near future, stay tuned!

Want to see the arbotiX in action? Here is a quick video showing a basic Inverse Kinematics demonstration on Issydunyet!

Korean Robot Games Festival 2009

Tuesday, September 1st, 2009

Our friends across the Big Pond at Robosavvy were lucky enough to visit the Korean Robot Festival this year. They took tons of pictures and shot a lot of video showcasing some of the world’s top humanoid competition robots! From slightly modified Robonova and Bioloid bots, to fully custom towering humanoids, all shapes and sizes showed up to compete. Pedro from Robosavvy did an amazing job of documenting his time there in this forum thread, anyone interested in humanoid robots will be delighted to check it out.

The thread linked above has the full details, but this video stood out to me as awesome; it’s a custom built humanoid using AX-12 servos. Check out how quick and agile it is!

Hagetaka: A Bipedal Combat Robot

Thursday, April 16th, 2009

Remember when we teased you with a stack of RX-64 servos? Well its time to unveil a bit more of what we’re working on for the upcoming Mech Warfare competition at Robogames 2009. Meet Hagetaka; a 7DOF per leg biped built around the powerful RX-64 servo from Robotis. This robot boasts 14 RX-64s, 2 RX-28s, a custom aluminum chassis machined by sponsor Big Blue Saw, an onboard linux based Gumstix computer with a PS3 Sixaxis controller , a WiFi video server using a Headplay Personal Cinema System for remote piloting, and of course dual automatic airsoft guns. Video and more info will be available in the near future, and be sure to check out the June issue of SERVO magazine for the first in a series of articles detailing the build process of this Mech.

Click for larger image.

Want to win a Bioloid? Announcing the TRC Tutorial Contest!

Friday, March 27th, 2009
Time flies! It’s that time again to officially announce the next round of the Trossen Robotics Community (TRC) Contest. We had quite a bit of success with our previous Project Contests and a lot of very cool entries, however we are going to mix things up this time.
This round is going to be a Tutorial Contest , and is quite a bit different from our previous contests. Think of it as an ‘Instructables meets How Stuff Works’ style contest: We want you to submit entries in the form of a detailed step by step ‘How-To’ or Informative Tutorials.
We’re going to be asking a lot more of our participants this round, so we have raised the stakes and are giving away our biggest prizes yet! Without further ado here are the prizes being offered for this round!
1st place

bioloid


Bioloid Comprehensive Kit:


2nd place



Bioloid Beginner Kit:


3rd place


ollo


Robotis Ollo Bug Kit
:

  • New Beginner Robotics Kit from Robotis!
  • Reconfigurable, modular design
  • Tons of parts to build with!
  • Instructions to build 4 different robots included
  • Remote controlled
  • Highly descriptive well documented instructions


You’re probably asking: “Well what’s the catch?” We won’t lie, we’re going to make you work for it and put your knowledge to the test!

Here are some examples of what types of tutorials we’re looking for:

  • What is a gyroscope/accelerometer/analog or digital signal?
  • How do servos/DC Motors/Batteries work? (explain inner workings, control, show example code, etc)
  • Choosing the right (Microcontroller/DC Motor/Sensor) for the job.
  • How to setup an Arduino/Xbee Communication/Basic Stamp. (basic projects with example code, videos, etc)
  • How to control a robot wirelessly. (many different methods of going about this, pick one and elaborate!)
  • Theory of Inverse Kinematics, Dead Reckoning, Spacial Mapping, etc.
We’re looking for well written, detailed entries that a beginner could read through and learn from. The emphasis on this is creating valuable tutorials and FAQs that the community as a whole can benefit from. Diagrams, pictures, source code, practical applications, text references and examples are welcomed and strongly encouraged. Plagiarism will not be tolerated, please cite any reference materials used. We are not looking for build articles during this round.
Entries will also be judged in a different manner than before: Contestants are encouraged to post as many tutorials as they like; in fact, the more tutorials submitted, the more points they receive towards their final score. Now that said, quality is greatly valued over quantity. One detailed, well written tutorial will hold more weight than five mediocre ones, but if you post numerous well written tutorials you’re going to be in very good shape.

Previous project submissions were based out of our Project Showcase forum, but this time all submissions must be entered into the Tutorial section.

Please visit our Project Contest Page to learn more about the contest, how to enter and for the official rules and guidelines. Somebody is going to be a proud new owner of a Bioloid Comprehensive Kit, Bioloid Beginner Kit, or Ollo Bug Kit, will it be you?

Big Pictures, Big Robots!

Monday, March 9th, 2009

Boston.com published a great article featuring a wide variety of robots around the world. If you like robots, and you like big pretty pictures of robots, you definitely have to check it out. In style with the article, I’ll keep this short and let you check out the pictures yourself!

Flying Wifi Robots: Friend or Foe?

Thursday, March 5th, 2009

Sure, the researchers may state they are intended for assistance in disasters… but these wifi network creating robots could just as easily be used to spread the reach of the dreaded Skynet! I have my doubts, but Engadget seems pretty sure that these robots have good intentions. Time shall tell!

Researchers at Germany’s Ilmenau University of Technology are developing flying quadcopter robots that can be used to form a self-assembling ad-hoc wireless network in the event of disaster. Built with off-the-shelf parts (including VIA’s Pico-ITX hardware and a GPS unit) the robots are designed to provide both mobile phone and WiFi access — and they can do it far more quickly than a technician on the ground might be able to. The device comes in a kit for €300 (about $380), which includes all but the battery — the batteries currently run around €1,000 (over $1200) and only offer up 20 minutes of flight time. Once the device has found a perch, however, it can operate for “several hours.”


Full story via Engadget.