We’re good friends with the folks over at Vanadium Labs; some very talented people who have been in the robotics game for quite awhile but have just now established their official company. This is great news for the robotics community however, as they have some pretty amazing products on the horizon. One product in particular is the new arbotiX Robocontroller, an advanced Open Source microcontroller tailored for the Bioloid system and AX-12+ servos.
The arbotiX robocontroller is an advanced control solution for small-to-medium size robots. It incorporates a powerful AVR microcontroller, XBEE wireless radio, dual motor drivers, and 3-pin servo-style headers for IO.
The arbotiX robocontroller is specifically designed to control robots built using Bioloid servos, although it is also a very high-end solution for powerful rovers. It is not intended to be a drop-in replacement for a CM-5, rather it is intended as a high level development tool for building more sophisticated robots.
So what we have here is an Arduino IDE compatible microcontroller with a plethora of I/O, plug and play capable with AX-12 servos, and an Xbee Wireless Link to your PC. It’s also worth mentioning that this was the controller used in the robot that won Year 1 of Mech Warfare, Issydunyet. For more information on the controller check out the Vanadium Labs website.
Trossen Robotics will be exclusively distributing this exciting and powerful new Robocontroller with an estimated release date of Mid-October 2009. We’ll have more details in the near future, stay tuned!
Want to see the arbotiX in action? Here is a quick video showing a basic Inverse Kinematics demonstration on Issydunyet!
We came, we conquered. Mech Warfare’s first year at Robogames 2009 was a success. We had a professional video crew on hand to record the action from multiple synchronous security cameras mounted within the arena, and even threw our interns inside during a few matches. This video is a highlights compilation of some of the robots that competed, enjoy!
Who doesn’t like free stuff? XMOS is offering some development kits of their new event driven parallel processors to qualified parties and individuals. These controllers looks like they pack a punch in terms of features and processing power and would make an awesome robotics controller! If you’re interested, check out the forum post by XMOS and answer the requested questions. Definitely shows some promise, check out the forums and the videos below for more info.
XMOS event driven processors allow you to execute code in parallel which could open up a number of possibilities to evolve your robots “mind” to the next level!
I have some development kits to give away potentially, but before I give away all the details, I just wanted to see if there was any interest.
People have made some cool stuff with our tech before (See videos).
Some details of the processor itself which will be on the dev kit (to be released soon):
- Single core device (Although we do have quad core versions – ask me)
- 400 MIPS per core.
- 8 Threads per core.
- 64Kb RAM
- 8KBytes OTP memory for applications, boot code or security keys, with security mode
- 64 user I/O pins
- Support for high performance DSP (32 x 32 → 64bit MAC) and cryptographic functions
- Time aware ports provide up to 10ns timing resolution
- Designs implemented using a software-based design flow (can program in C or XC – very similar to C but with support for extras such as parallel execution)
- Scalable – can connect many kits together for crazy amounts of processing power using Xlinks.
Remember when we teased you with a stack of RX-64 servos? Well its time to unveil a bit more of what we’re working on for the upcoming Mech Warfare competition at Robogames 2009. Meet Hagetaka; a 7DOF per leg biped built around the powerful RX-64 servo from Robotis. This robot boasts 14 RX-64s, 2 RX-28s, a custom aluminum chassis machined by sponsor Big Blue Saw, an onboard linux based Gumstix computer with a PS3 Sixaxis controller , a WiFi video server using a Headplay Personal Cinema System for remote piloting, and of course dual automatic airsoft guns. Video and more info will be available in the near future, and be sure to check out the June issue of SERVO magazine for the first in a series of articles detailing the build process of this Mech.
You’ve all seen and heard the robotic dancing sensation known as Keepon, and now you can own one!
When Keepon first debuted, bouncing along to Spoon’s “I Turn My Camera On”, the tech community went nuts! The simple, cute external appearance of this robot and it’s natural ability to bop along with music was an instant hit on Youtube. Unfortunately, beneath that elastic yellow skin was well over $20,000 worth of cutting edge robotic technology, putting this awesome robot out of reach of its fans. We saw this as a problem and answered the call to unite Keepon and it’s millions of fans globally!
After many months of painstaking R&D, Trossen Robotics is proud to announce the Low Cost Dancebot! Once only available to universities as a high end social development research robot, we are now offering the affordable yet equally groovy Low Cost Dancebot! This easy to build kit only takes minutes to put together, another minute to put on the Spoon song of your choice, and within seconds your Low Cost Dancebot! will be dancing along to the beat. Be the envy of your coworkers with this ultimate desktop gadget! Show off to your friends, amaze your family, and impress your employer!
The Roboard RB-100 is a new breed of robotics controller: a fusion of a traditional microcontroller and a full function computer. Think of it as an OS capable microcontroller on steroids, boasting a 32bit x86 CPU running at 1000MHz and 256MB DRAM. The ability to load an operating system of your choice and have direct access to I/O, Comm ports, USB, and networking opens this controller up to a wide range of robotics based applications. Our Roboard Starter Kit comes with just about everything you need to implement this feature rich controller in your next robotics project! All you need to supply is a 1-2gb Micro-SD card to load an OS onto, 6-24v, and a robot!
Boston.com published a great article featuring a wide variety of robots around the world. If you like robots, and you like big pretty pictures of robots, you definitely have to check it out. In style with the article, I’ll keep this short and let you check out the pictures yourself!
Sure, the researchers may state they are intended for assistance in disasters… but these wifi network creating robots could just as easily be used to spread the reach of the dreaded Skynet! I have my doubts, but Engadget seems pretty sure that these robots have good intentions. Time shall tell!
Researchers at Germany’s Ilmenau University of Technology are developing flying quadcopter robots that can be used to form a self-assembling ad-hoc wireless network in the event of disaster. Built with off-the-shelf parts (including VIA’s Pico-ITX hardware and a GPS unit) the robots are designed to provide both mobile phone and WiFi access — and they can do it far more quickly than a technician on the ground might be able to. The device comes in a kit for €300 (about $380), which includes all but the battery — the batteries currently run around €1,000 (over $1200) and only offer up 20 minutes of flight time. Once the device has found a perch, however, it can operate for “several hours.”
One of the single most challenging aspects of home navigation for robots has to be tackling stair climbing. While humans can move up and down without much trouble at all, even advanced robots such as ASIMO still have ‘issues’. The UCSD Coordinated Robotics Lab has developed a pretty efficient and simple (in concept, not execution) way of doing just that with their iLean Robot. Check out the video below to see how it works, really an amazing thing to see executed so well!