Archive for the ‘Military’ Category

VIPeR a Portable Combat Robot

Tuesday, March 13th, 2007
viper-full

I am most impressed by the fact that the wheels on this robot can actually change shape. Check out the mini flash clip or video after the jump.

This portable, lightweight robot is operated by a single operator, and is designed to negotiate obstacles typical of an urban environment, such as climbing stairs and rubbles, when performing surveillance, reconnaissance and support troops in urban warfare missions. The vehicle uses the “Galileo Wheel”, a patented system developed by Galileo Mobility Instruments ltd. that allows automatic back and forth conversion among a wheel configuration, a track configuration and a special stair climbing configuration. (View a video showing the performance of the Galileo robot prototype).

via defence-update.com via digg post

Robots from Boston Dynamics

Wednesday, February 28th, 2007

Boston Dynamics makes some very advanced robots !

Darpa wants Luke’s replacement hand from Star Wars

Wednesday, February 21st, 2007
robotics limb

Thought-controlled robotic limbs were only the beginning.

hand.jpgScientists have had a string of remarkable successes lately, taking signals from the brains of monkeys and men, and using them to move mechanical arms.

Darpa, the Pentagon’s blue-sky research division, now wants to ratchet that work up about ten notches, by developing a “neurally controlled artificial limb that will restore full motor and sensory capability to upper extremity amputee patients. This revolutionary prosthesis will be controlled, feel, look and perform like the native limb.”

read more

via Digg

Chaos: one tough robot – run for your life

Monday, January 22nd, 2007
chaos
chaos

I would not want this robot chasing me. Nothing stops it. Watch the videos after the jump to see it climb over piles of rubble and branches with ease.

From the Chaos Homepage:

Chaos is a highly mobile small robot useful for

* explosive ordinance disposal,
* surveillance,
* reconnaissance,
* search and rescue,
* hauling gear,
* and other dull, dirty, or dangerous tasks.

Chaos is a robotic platform with four configurable and independently controlled tracks. Its superior design allows it to go where no other robotic platform of its size can go. It can handle terrain like stairs, train tracks, rubble piles, gravel, and steep grades of loose debris. It was recently tested at Disaster City in Texas, the premier search and rescue training ground. There, in some of the most difficult terrain a robot will encounter, Chaos demonstrated its superior mobility.

The basic Chaos platform is fully JAUS compatible. Chaos has the volume and weight capacity to handle the load of a wide variety of sensor and robotic payloads, such as an arm for EOD applications or senosrs for Hazmat situations. Chaos is supplied with Mobi, ASI’s handheld operator control unit (OCU) loaded with the Mobius software, the universal control for unmanned systems. Mobius supports operational modes from simple tele-operation to multi-vehicle autonomous behavior. The combination of Chaos, Mobi, and Mobius provides the power, design and intelligence you need to go to more places.

chaos_four_tracks

Chaos, weighing in at 120 pounds, has more torque and payload capacity than any robot in its weight range. It uses an ultra-efficient motor and gearbox design to acheive impressive torque and an operational battery life of three hours. The design also makes it very quiet, with virtually no gear or motor noise.

Chaos uses an ultra-efficient motor and gearbox design to acheive impressive torque and an operational battery life of three hours. Chaos is modularly designed, so all components (tracks, arms, drive modules, electronics module, battery, and chassis) can easily be replaced in the field. All components connect solidly together without any velcro or straps.

VIA slashgear, technabob

Chaos homepage

An Ear for Snipers – A new robotic head can pinpoint the location of enemy shooters

Thursday, January 18th, 2007
sniper

The RedOwl is a robotic head that looks more like a PowerPoint projector than a sharpshooter’s worst enemy. But don’t let its Circuit City appearance fool you: Controlled by a laptop-wielding soldier, the RedOwl’s superior senses can read a nametag from across a football field and identify the make and model of a rifle fired a mile away simply by analyzing the sound of the distant blast. And soon it could be putting its powers to use in Iraq.RedOwl’s developer, Glenn Thoren, now a director at Insight Technology in Londonderry, New Hampshire, says several prototypes have finished an intensive 10-week field test at Fort Benning in Georgia. Given the defense department’s budget approval early this year, he hopes the $150,000 sniper-finders will be in Iraq by this spring. The robot’s mechanical ears were originally designed to improve hearing aides. But Thoren, then with Boston University’s Photonics Center, which heads the RedOwl project, thought up a new application after learning of a spike in sniper activity surrounding Iraqi hotspots like Abu Ghraib prison… read more

via zinzi & popsciÂ