We’ve been busily preparing for the iHobby 2009 show this week, but I figured I would share a little demo video of Giger. He now sports a TinyCylon eye from DaleWheat.com, and has a few new fighting moves up his sleeve, ready for some fights at Chibotica during iHobby! Walking gait is still obviously a work in progress, but what is being demonstrated in the video is the ability to pan/tilt the torso while walking, which makes the walking gait even more unsteady. Enough jabbering, here’s a bit of video!
Archive for the ‘Mech Warfare’ Category
Giger is ready for iHobby!
Wednesday, October 21st, 2009Giger: RX-64 Based Custom Humanoid
Wednesday, September 30th, 2009With my Hagetaka project on hiatus (eventually being rebuilt using EX-106s), my efforts had been diverted to a simpler and more manageable design. Originally intended as a last minute work around for Robogames, this project ended up being a permanent effort, and one that I’ve grown rather fond of.
Giger is a 24″ custom 24 DOF Humanoid using 16 RX-64 and 8 RX-28 Dynamixel Servos, weighing in at 9lbs total. He uses the same Gumstix based onboard controller that Hagetaka did, designed by Farrell Robotics, and is powered by two 1900mAh 4S LiPo batteries.

Walking gait is being refined, I’ll have video in the near future but much progress has been made. If all goes well, I’ll have him up and running for iHobby 2009 next month! Here are a couple of pictures, for the full set that we took check out my gallery in the TRC!

Can You Smell What Lynxmotion Is Cooking?
Friday, September 11th, 2009Our good friends over at Lynxmotion have been a force to be reckoned with for well over a decade in the robotics industry; producing some truly inspiring and amazing robots over the years. My first ‘real’ robot was a Lynxmotion Hexapod 1 (the 3 servo variety) that I picked up back in 1997, and their product lines were one of the driving forces that got me addicted to robotics.
Well, they’ve impressed me yet again; Lynxmotion owner Jim and his son James, being robot enthusiasts and likewise fans of the Mechwarrior franchise, were intrigued with the Mech Warfare competition. Specifically they loved the biped aspect of it and so they set out to create a low cost competitive platform for Mech Warfare, and succeeded. Nicknamed ‘Hunchback’ and based around their BRAT biped platform, this is turning out to be one of the lowest cost and straight forward platforms for the competition. Currently there is a work-in-progress tutorial showing the build and code, and it looks like we have a very high chance of being treated to a complete kit allowing you to build your very own. If you’re interested in seeing how it progressed from prototype to near final revision, check out the project thread over on the Lynxmotion forums. Check out the following video of the Hunchback in action!
Robots with Friggin Laser Beams on their Heads!
Monday, August 31st, 2009Giving robots weaponry seems to be a recurring theme with humanity’s technological progression in robotics. Not that there is anything wrong with that; it’s not like something could ever go wrong in the future. Right?
In America, we’ve got Mech Warfare which implements archaic Airsoft guns and rockets. Japan however, has decided to step it up a notch and have equipped their robots with lasers. Building exploding, blindness causing, movie theater annoying lasers of destruction. To add insult to injury, they’ve even adding awesome PEW PEW PEW noises to their lasers! Why must you taunt us Japan, why?!? Not only do you make cooler robots, but now you’re giving them lasers. Totally not fair. The Robot BLASER Battles are definitely awesome though, check out their 2nd annual competition video below:
Mech Warfare 2009 Highlights Video
Tuesday, August 11th, 2009We came, we conquered. Mech Warfare’s first year at Robogames 2009 was a success. We had a professional video crew on hand to record the action from multiple synchronous security cameras mounted within the arena, and even threw our interns inside during a few matches. This video is a highlights compilation of some of the robots that competed, enjoy!
Trossen Robotics Community Lounge @ Robogames 2009
Thursday, July 16th, 2009We had a blast at Robogames 2009 and had quite a few of our Community members show up and hang out in our lounge. Robots were battled, discussed, and otherwise shared! We cannot wait until next year, and we hope to see more of you there. Here is a quick highlight video showing some of the lounge and the attending members, as well as some of our member’s robots interacting with the crowd.
Some TRC Projects to keep an eye on!
Tuesday, July 7th, 2009We’re rather lucky that we have such a large group of talented individuals in our community who are willing to share their progress and projects! A few recent projects have caught my eye so I wanted to share the wealth; some pure robotic goodness to be had here.
First up we have the infamous Zenta’s quadrapod robot project: Felix! Zenta has recently picked this project back up and teased us with a quick video of the bot walking. You can certainly see its Big Dog inspired walking gait and design.
WGhost9 is impressing us all with the professional machining skills displayed in his latest project, Beetlejuice. This is a hybrid hexapod with wheels on each end actuator, coupled with some fantastic craftsmanship on the shell that gives it a great aesthetic. It’s still a work in progress, but he is detailing each step he is taking in the project, definitely something to keep an eye on.
And last but not least, newcomer Upgrayd is detailing his quadrapod Mech build, “Second Amendment“. He is also posting as the project progresses, so the readers get a chance to see the thought process and inevitable mistakes that come along with any big robotics project. Can’t wait to see this bot at next year’s Mech Warfare!
iPhone controlled Mech?
Thursday, July 2nd, 2009After Year 1 of Mech Warfare, the competitors are busy working away to improve their bots, control scheme, weapons, etc… so it was only a matter of time before we would see someone adapting an iPhone to control their mech. Seeing as though the iPhone can be used for anything (Defibbing people, saving kittens from trees, backup generator for your house, etc), remotely controlling walking combat robots was the next logical step.
Builder Mannyr7 and his mech project CLYDE suffered some last minute setbacks that prevented him from competing at Year 1 (though he did show up to cheer us on and impress us with his professional airsoft gun setup), however he has taken the time to write up a tutorial and shoot a video on his latest iPhone control scheme. Definitely check it out, as its applicable to a variety of robots!
Initial Mech Warfare Coverage
Tuesday, June 23rd, 2009We want to apologize for being so quiet, but Robogames and the subsequent chaos of getting caught up has taken us all by a storm. We’ll be making up for it by posting a ton of content in the next few days.
Year 1 of Mech Warfare turned out great, better than expected for a first year competition. We came, we conquered, and more than anything we learned a LOT. Seven robots total showed up, though Murphy’s Law was in full effect and we only had 4 running consistently. That said, everyone involved still had a ton of fun, and Botjunkie and Society of Robots were there covering the action. Here are two quick highlight videos they put together, stay tuned for the official Mech Warfare coverage video from multiple in-arena cameras in the near future!
Video coverage from Botjunkie:
And video coverage from Society of Robots:
Hagetaka: A Bipedal Combat Robot
Thursday, April 16th, 2009Remember when we teased you with a stack of RX-64 servos? Well its time to unveil a bit more of what we’re working on for the upcoming Mech Warfare competition at Robogames 2009. Meet Hagetaka; a 7DOF per leg biped built around the powerful RX-64 servo from Robotis. This robot boasts 14 RX-64s, 2 RX-28s, a custom aluminum chassis machined by sponsor Big Blue Saw, an onboard linux based Gumstix computer with a PS3 Sixaxis controller , a WiFi video server using a Headplay Personal Cinema System for remote piloting, and of course dual automatic airsoft guns. Video and more info will be available in the near future, and be sure to check out the June issue of SERVO magazine for the first in a series of articles detailing the build process of this Mech.