I’m not at all exaggerating; Loki, a 4 foot tall 40lb ‘Domestic Style’ robot looks far better than anything I have seen produced for commercial sales.
Beautiful aesthetics aside, functionally it is one of the most impressive and polished PC based robots I’ve ever seen as well; custom software that handles object recognition, mapping and navigation, as well as voice commands, just to name a few. If all of that wasn’t impressive enough, creator Dave Shinsel has the schematics, documentation and even source code available on his site! Definitely check out Dave’s entire site, he has an impressive body of work, and his Youtube Page has some very cool videos demonstrating Loki in action.
In March we announced that our contest would go in a different direction this time and with even bigger prizes:
This round is going to be a Tutorial Contest , and is quite a bit different from our previous contests. Think of it as an ‘Instructables meets How Stuff Works’ style contest: We want you to submit entries in the form of a detailed step by step ‘How-To’ or Informative Tutorials.
We had a good amount of solid entries in our first Tutorial Contest so picking our winners was a not an easy ordeal. Our entries covered many different topics, from electrical and soldering basics to more advanced robotics navigation tutorials. We highly suggest that you take a look at our Tutorials Section, there is a lot to be learned and if you have knowledge to share we highly encourage it.
Jes1510 submitted some ‘back to the basics’ tutorials which were well documented, easy to read through, and really helpful for the beginning robot hobbyist! He’ll be walking away with an Ollo Bug Kit!
Pi Robot amazed us with two extremely detailed, professional tutorials that cover some very advanced robotics applications by breaking it down into more digestible bite sized pieces. Both are excellent pieces of literature, definitely worth a read through! Pi Robot will be walking away with a Bioloid Beginner Kit for his contributions!
lnxfergy was determined to win 1st prize! He submitted awesome tutorial after awesome tutorial covering some pretty major aspects of robotics. All of these tutorials are very helpful for beginners and even more advanced builders can take something from them. From practical navigation systems to controlling AX-12 servos, lnxfergy demonstrated an amazing grasp of current hobby robotics technology, and was kind enough to share that knowledge with us. For his massive effort, he will be awarded with a Bioloid Comprehensive Kit!
We want to thank everyone involved with our first Tutorial Contest! Determining the winners was not easy, as there were many great tutorials to browse through. Again, we highly recommend you check out our Tutorials section, as there is a lot to be learned! Stay tuned for an announcement on our next round of contests!
The creator doesn’t have a name for it past “Little Walking Robot”, but I could think of a few words to describe it: Awesome, sexy, and umm, Awesome.
No but really, thing thing is a marvel of aesthetic design and function. Has a Steampunk meets “Dragoon from Starcraft” look to it. The inventor of this beauty has a well written blog detailing his progress and some of the problems he ran into along the way, as well as a Flickr photo set. This bot is all custom built from a mix of hand-built parts, as well as some waterjet steel frame components from our friends at Big Blue Saw.
Check the video below for the bot in action, big thanks to Big Blue Saw for the scoop.
We’re rather lucky that we have such a large group of talented individuals in our community who are willing to share their progress and projects! A few recent projects have caught my eye so I wanted to share the wealth; some pure robotic goodness to be had here.
First up we have the infamous Zenta’s quadrapod robot project: Felix! Zenta has recently picked this project back up and teased us with a quick video of the bot walking. You can certainly see its Big Dog inspired walking gait and design.
WGhost9 is impressing us all with the professional machining skills displayed in his latest project, Beetlejuice. This is a hybrid hexapod with wheels on each end actuator, coupled with some fantastic craftsmanship on the shell that gives it a great aesthetic. It’s still a work in progress, but he is detailing each step he is taking in the project, definitely something to keep an eye on.
And last but not least, newcomer Upgrayd is detailing his quadrapod Mech build, “Second Amendment“. He is also posting as the project progresses, so the readers get a chance to see the thought process and inevitable mistakes that come along with any big robotics project. Can’t wait to see this bot at next year’s Mech Warfare!
After Year 1 of Mech Warfare, the competitors are busy working away to improve their bots, control scheme, weapons, etc… so it was only a matter of time before we would see someone adapting an iPhone to control their mech. Seeing as though the iPhone can be used for anything (Defibbing people, saving kittens from trees, backup generator for your house, etc), remotely controlling walking combat robots was the next logical step.
Builder Mannyr7 and his mech project CLYDE suffered some last minute setbacks that prevented him from competing at Year 1 (though he did show up to cheer us on and impress us with his professional airsoft gun setup), however he has taken the time to write up a tutorial and shoot a video on his latest iPhone control scheme. Definitely check it out, as its applicable to a variety of robots!
Who doesn’t like free stuff? XMOS is offering some development kits of their new event driven parallel processors to qualified parties and individuals. These controllers looks like they pack a punch in terms of features and processing power and would make an awesome robotics controller! If you’re interested, check out the forum post by XMOS and answer the requested questions. Definitely shows some promise, check out the forums and the videos below for more info.
XMOS event driven processors allow you to execute code in parallel which could open up a number of possibilities to evolve your robots “mind” to the next level!
I have some development kits to give away potentially, but before I give away all the details, I just wanted to see if there was any interest.
People have made some cool stuff with our tech before (See videos).
Some details of the processor itself which will be on the dev kit (to be released soon):
- Single core device (Although we do have quad core versions – ask me)
- 400 MIPS per core.
- 8 Threads per core.
- 64Kb RAM
- 8KBytes OTP memory for applications, boot code or security keys, with security mode
- 64 user I/O pins
- Support for high performance DSP (32 x 32 → 64bit MAC) and cryptographic functions
- Time aware ports provide up to 10ns timing resolution
- Designs implemented using a software-based design flow (can program in C or XC – very similar to C but with support for extras such as parallel execution)
- Scalable – can connect many kits together for crazy amounts of processing power using Xlinks.
We want to apologize for being so quiet, but Robogames and the subsequent chaos of getting caught up has taken us all by a storm. We’ll be making up for it by posting a ton of content in the next few days.
Year 1 of Mech Warfare turned out great, better than expected for a first year competition. We came, we conquered, and more than anything we learned a LOT. Seven robots total showed up, though Murphy’s Law was in full effect and we only had 4 running consistently. That said, everyone involved still had a ton of fun, and Botjunkie and Society of Robots were there covering the action. Here are two quick highlight videos they put together, stay tuned for the official Mech Warfare coverage video from multiple in-arena cameras in the near future!
And as the saying goes, a picture is worth a thousand words, so we’re at least in the million “word” range with our TRC Gallery. Over the past year our Community has grown considerably, and with it a really awesome collection of pictures from our various members’ projects! We highly recommend a look through if you’re the robot savvy type. Here are just a few choice pics to share:
I remember being blown away at how strong my first hobby servos were when I built my Hexapod 2 from Lynxmotion about 12 years ago. In comparison, they were literally just a fraction of the strength of modern digital servos, and the gap widens even further when put up against a robotic actuator such as the RX-64 Smart Actuator.
I was working on my mech Hagetaka the other night and made the mistake of grabbing at the robot to stabilize it while it was moving, and managed to graze my finger in one of the joints. It drew blood and immediately reminded me that working with these types of servos was an entirely different ballgame than your standard hobby servo. With that in mind, we put together a little demonstration video of just how powerful these servos can be! Enjoy!
Remember when we teased you with a stack of RX-64 servos? Well its time to unveil a bit more of what we’re working on for the upcoming Mech Warfare competition at Robogames 2009. Meet Hagetaka; a 7DOF per leg biped built around the powerful RX-64 servo from Robotis. This robot boasts 14 RX-64s, 2 RX-28s, a custom aluminum chassis machined by sponsor Big Blue Saw, an onboard linux based Gumstix computer with a PS3 Sixaxis controller , a WiFi video server using a Headplay Personal Cinema System for remote piloting, and of course dual automatic airsoft guns. Video and more info will be available in the near future, and be sure to check out the June issue of SERVO magazine for the first in a series of articles detailing the build process of this Mech.