Archive for the ‘Announcements’ Category

Now Taking Pre-Orders on the Bioloid Boomerang ZigBee Controller!

Wednesday, October 22nd, 2008

Bioloid users have been drooling over these controllers since they were first announced at Robogames 2008! Well, the time is nigh to get your robot a fix, the Bioloid Boomerang Zigbee Controllers are due on our next shipment! These controllers finally put wireless Bioloid control into user’s hands, enabling easier participation in humanoid kung-fu, soccer, and stairclimbing.

We are now accepting Pre-Orders, with an expected arrival date of November 15th, 2008. They come in two flavors, one with a set of Zig-100s, and one without (if you already had purchased a pair previously). Get em while they’re hot!

Announcement: Next Round of the TRC Project Contest

Wednesday, October 8th, 2008

It’s that time again to officially announce the next round of the Trossen Robotics Community (TRC) Project Contest. With the success of last round, it was obvious many preferred the idea of offering Robots as prizes, so we’re doing it again:-)

The goal of the TRC Project Contest is to encourage technological creativity, innovation and ingenuity through these talented individual’s unique projects. We invite everyone to help spread the word about this contest announcement to help encourage others to show off their talent.

1st place


Pleo™ from UGOBE


Includes:

  • 2 32-bit Microprocessors – central and image processing
  • 4 8-bit Subprocessors – motor control
  • 14 motors
  • Over 100 custom-designed gears
  • Camera-based vision system – light detection and navigation.
  • 2 Microphones – binaural hearing
  • 8 Skin sensors – head, chin, shoulders, back, legs
  • 4 Foot switches – surface detection
  • 14 Force-feedback sensors – one per joint
  • Orientation tilt sensor – body position
  • Infrared mouth sensor – object detection
  • SD card slot – Pleo add-ons

2nd place




WowWee RS-Media™

Features:

  • Chest Mounted LCD Screen
  • PC-Based Editing Suite
  • Head Mounted Camera
  • Sonic Sensors
  • 40MB Memory w/ SD upgrade slot
3rd place




Wowwee Roboquad™

Modes:

  • IR Vision w/Scanning features
  • Head mounted LED’s
  • 72 Preprogrammed Functions
  • Multiple Modes
  • Advanced Motion Control
  • Personality Settings
  • Light Sensor
  • Sound Sensor

Please visit our Project Contest Page for further information and instructions on how and where to submit your project. Somebody is going to be a proud new owner of a WowWee Roboquad, RS-Media, or… wait for it…. a PLEO from UGOBE. Will it be you?

We Cleaned Out Our Lab! Killer Grab Bag Deals To Be Had!

Tuesday, September 30th, 2008

We started hearing strange noises coming from our Laboratory late at night (Well, I guess I did since I’m the only one who works late around here, I work with slackers). Upon further inspection the next day, we noticed our ridiculously large stockpile of random electronic parts and mechanical gizmos had apparently gained sentience and was attempting to build itself into a robotic monstrosity that would surely slay us all. Well, that’s what I think anyway, my fellow coworkers think I should leave the office and go home at some point.

Needless to say, it was time to clear out our stockpiles of random stuff. We slaved away, battling robotic creations from the night and finally getting our Lab back under our control. So, we’re unleashing our piles of parts into the general public at a deep discount, in hopes that our Lab stays under our control.

Check out our new limited quantity Grab Bags in our Garage Sale Section!

This is the pack-rat/tinkerer/engineers dream come true! More deals are to come, but get em while they’re hot because at these prices our Grab Bags will not last long!

Here is a sample of a few items we have up for grabs:

Flex Force/Touch/Pressure Sensor Grab Bag!

Handfuls of Rotary Encoders!

More Sprockets and Chain than any human could ever need!

A variety of motor and servo controllers!

This is just a sample of what we have up for grabs, so be sure to check out our Garage Sale section soon!

Trossen Robotics announces their new Educational Division

Tuesday, September 23rd, 2008

Trossen Robotics has announced the launch of their new Educational Robotics Division. Building upon the knowledge and experience they have gained as a premiere US distributor of robotic kits and components, they have hand picked the best robotic kits tailored specifically for classroom use to create a one stop shop for educators using robotics in education.

Trossen Robotics has been committed as a business to helping robotics advance in the US and the new Education Division is another step forward in their continuing efforts. Matt Trossen, founder, explains their focus, “We saw that one of the major stumbling blocks for educators interested in integrating robotics into their classrooms was the fragmentation of all the products and information. Our goal is to be a top notch aggregator for teachers. To create a single comprehensive storehouse of products, guides, and information.” Matt also comments on the future of the division and goals for robotics in education, “We will continue to integrate curriculum and project manuals into the site for educators to use. Our goal is to make it as easy as possible for educators to research, choose, and integrate robotics into their curriculum. This is the way we as a company can help keep US schools cutting edge which is as important now as has ever been.”

Offerings from Parallax,  Robobuilder, Robotis, Lego Mindstorms, Robotics Connection, VEX and many more are displayed in an easy browse format. Educators are informed of exactly what each kit brings to the classroom, what difficulty and scope of work is involved in the projects, and what their students can expect to bring out of the learning experience. Ordering from the same source also saves educator’s time and valuable education dollars.

What do robots bring to the classroom? Robotics is an exciting field of science that brings mechanical, electronic, and even software engineering together. Skills ranging from physics, mathematics, mechanical design, soldering, programming, logic, and teamwork are built as a foundation of knowledge that has limitless potential. Students get to see the results of their work in a tangible, physical application of science as their projects come to life.

Trossen Robotics cordially invites educators, students, and parents alike to visit their new Educational Division.

Download the PDF version of this announcement here.

American Maker in Chicago!

Friday, September 5th, 2008

Calling all Chicago area inventors! Come to the Museum of Science and Industry and show off your inventions! Compete for fame and fortune, conquer the legions of fellow tinkerers, and claim your right as King of the Geeks!

Okay just kidding, this is a friendly competition, but the winner does get a cash prize and publication in a future issue of MAKE. Info below:

American Maker Logo

On Saturday, September 20th at the Museum of Science and Industry, the editors of MAKE will be organizing a “show-and-tell” program called American Maker. The goal of American Maker is to showcase grassroots innovation from Chicago-area makers. We’re looking for makers who are working on cool projects and whose work has the potential to benefit others. We believe that makers are a leading force in grassroots innovation — where individuals decide to create something new.

American Maker is a friendly competition and the winner will be awarded a $500 cash prize plus publication in a future issue of MAKE.

If you’d like to participate and show what you make at this event, you can submit a project at:

http://www.makezine.com/american/

You are also welcome to come on Saturday, September 20th and join us in the audience. American Maker is part of Lab Fest, which kicks off Science Chicago at the Museum of Science and Industry. American Maker will run from 10 a.m. to 4 p.m. on September 20th. Admission to the museum is free on that day.

We hope to see you there!

Cheers,
The MAKE Team
cs@readerservices.makezine.com
http://makezine.com/account

August TRC Project Contest Winners!

Monday, August 4th, 2008

As many of you may know by now, the Trossen Robotics crew hosts project contests every few months, where the winners are awarded in lavish gifts such as gift cards, robot kits and trips to the Playboy Mansion! (Okay, maybe not that last one. But they won’t put me in charge of picking out the prizes for some reason)

Members of the Trossen Robotics Community (TRC) face off in a battle of robotic wits! They come up with all sorts of great inventions, document their work, take a ton of photos and video, and post about it all in our Project Showcase Forum in hopes of being whisked off to the Playboy Mansion! Or…in hopes of winning fantastic robo-prizes.

The time is nigh to pick out winners. We flew our finalists out here to Chicago and determined the winners the only fair way we could think of: We put their projects on the sidelines, armed the inventors with sporks, and threw them into an arena in a fight to the death ala Bloodsport! (Okay, again, this didn’t happen.. who makes these contest rules anyway?) The TR crew locked wits in the discussion as to who would place these past few weeks. Heated public debates were held, dirt-throwing campaign commercials were made, friendships were torn apart… and in the end we finally came to an agreement. Without further ado, here are the runners-up and winners, in suspense-building ascending order!

- – - – - – - – - – - – - – - – - – - – - – -

Honorable Mention:
Swashbot!Flapper Fish!

Project: Swashbot(s) & Flapper Fish
Creator: CrabFu

You’re probably wondering: “Wait, why didn’t The Great Crabfu win??” Well, that’s exactly why. He’s too great! It wouldn’t be fair to let “Geppetto Emeritus” steal away first place, so we took him down a notch and gave him an honorable mention. This man might not even be human the way he produces robots, it seems like we had a new invention from him every other week! Keep em coming Crabfu!

Hex CNCHex CNCHex CNC

Project: Walking CNC Router Robot
Creator: Matt Denton

Matt Denton, animatronics whiz of MicroMagic Systems is known for his incredible hexapods. If you’re not familiar with them, I suggest you check them out here. Well simply walking, dynamically balancing, and snapping pictures of people to post on it’s site (yes, the robot has a website) wasn’t enough for this Hexapod. Matt went ahead and taught it how to be a CNC router. That walks. Flashbacks from “Runaway” aside, this project is really amazing and shows how far robotic technology is progressing. He went all out and cut a 3D image of a face out of foam using the robot’s I.K. engine alone. Big kudos!

- – - – - – - – - – - – - – - – - – - – - – -

Runners-Up:

Project: Butler Robot
Creator: airman00
Average Score: 7.1
Prize: $25 Gift Card to the Trossen Robotics Store

Everyone always wanted their own Rosie the Robot as a kid right? Well meet Chives the Butler Bot. Good ol’ Chives here can pour drinks, respond to voice commands, has onboard vision processing and can be controlled via laptop or iPod Touch! To make things better, you can even build your own. Airman00 wrote up a comprehensive step by step guide to build your very own robotic butler! He even is provided all of his code as open source. Great job!

RC Truck

Project: RC Truck Robot Conversion
Creator: Orac
Average Score: 7.3
Prize: $25 Gift Card to the Trossen Robotics Store

Leave it to one of our members to steal an R/C Truck from his kid and slap a computer on it. Regardless of this R/C Truck’s origins, its obvious that it is awesome. Orac took this car, modded it and added a fully functioning PC and a webcam to it. This not only gave it the option for off-road telepresence, it made it simultaneously chase and run away from orange colored balls. Like a puppy! A really ugly puppy. Made of plastic and metal.

Project: iLush Bartender
Creator: metaform3d
Average Score: 7.5
Prize: $25 Gift Card to the Trossen Robotics Store

Okay, first of all, this robot serves booze. Do we really need to continue as to why this kicks ass? Metaform3d impressed the judges at Robogames 2008 with his iLush Bartender, which serves up mixed drinks and is controlled via a touchscreen computer. He ended up walking away with a gold in the Bartending category (Yes, there is a robo-bartending category). Wow!

Project: RoboCam
Creator: Norris56
Average Score: 7.7
Prize: $25 Gift Card to the Trossen Robotics Store

This isn’t your average telepresence bot, creator Steve Norris took this one to the next level. Starting off with just an iCreate base, he built a very professional looking robot that can be driven from anywhere there is internet. That’s right, the entire robot can be remotely piloted from across the globe via a custom web interface that Steve designed. He even armed it with a laser to assist with depth perception (I thought lasers were only supposed to be mounted on sharks?) I guess our only question is, when can we buy one?

- – - – - – - – - – - – - – - – - – - – - – -

Third Place:

Project: XR-B3
Creator: lnxfergy
Average Score:8.7
Prize: Wowwee Alive Elvis

This cool little bot runs a custom microcontroller onboard that has a wireless link back to a computer, which handles the heavy lifting. And by heavy lifting we mean machine vision and room mapping capabilities. Not only is this impressive from a technical standpoint, it also has a very slick aesthetic, and overall a very impressive build quality to it. Be sure to check out the project page on this for more information and updates!

Second Place:

Project: AMOS-WD06
Creator: AMOS
Average Score: 9.3
Prize: Silverlit R/C X-UFO

This Hexapod is just downright impressive. The AMOS-WD06 (Advanced Mobility Sensor Driven-Walking Device) contains 21 actuators and 28 sensors and at its brain is a neural networked PDA. The programming behind this bot is what really makes it impressive as it is being designed to act and react like an insect. It exhibits Phototaxis, has a dynamic obstacle avoidance routine, will shy away from ‘predators’ and if you flip it on its back it can flip around and keep walking! We expect to see even more great things as this project develops.

First Place:

Project: Homebrew Wall-E
Creator: 4mem8
Average Score: 9.7
Prize: SG-5UT Robotic Arm

Well what can we say, we fell in love with this bot at first sight. We got to watch 4mem8 bring this guy to life and document every painstaking step that he took building this Wall-E robot from scratch. That’s right, this was not a kit, in fact he had the majority of it done far before the movie actually hit theaters and the toy stores were flooded with Wall-E merchandise. The robot itself is carved and crafted largely out of wood, and the rest from random parts found here and there… like a true ‘junk-bot‘ should be! 4mem8 has made a great contribution with his knowledge and experience in building bots, so we’re very proud present to him with the first place prize in this round of the TRC contest. Good job 4mem8! You earned it! Be sure to also check out 4mem8’s project on RoboCommunity.

- – - – - – - – - – - – - – - – - – - – - – -

We would like to take this time to congratulate and thank everyone who participated in this round of the contest. Not only have we seen some amazing projects entered, but we’ve gained some really incredibly talented members in our community as a result. We look forward to the next round of our contest, keep tuned in for more info. You can stay up to date on contest rules and regulations at the Trossen Robotics Project Contest page, and start posting your projects in our Project Showcase Forum.

They’re Heeeeeeere! RoboBuilder has Arrived!

Monday, July 28th, 2008

robobuilder is here

The RoboBuilder kits have arrived !!

You can find them in the catalog in the Humanoids section or the Full Robotics Systems section.

RoboBuilder is the new building block robot kit on the scene. Designed for robot enthusiasts and education alike RoboBuilder hits a sweet spot with feature packed kits at great prices. Its designers focused on form as much as function and the result is a great looking robot. The 5720T kit even sports translucent plastic with multicolored internal LEDs. You could take this little guy to the rave with you on the weekends!

Don’t let the streamlined good looks of RoboBuilder fool you. Beneath all that flash lurks plenty of substance. RoboBuilder is packed with advanced features not found on many of the other kits in the market such as: Precise PID Motion Control, distance detection, sound detection & speaker system, IR remote control included, Bluetooth upgradeable, and full-duplex drop-down UART serial communication on the smart actuators.

A common complaint in robotics is that too much time is often spent building robots and not enough is spent enjoying them. RoboBuilder solves this problem with their unique quick assembly joints which make assembly and design changes a breeze. Building is so easy that a complete humanoid takes less than two hours to assemble.

Once the robot is built there are multiple easy to use software interfaces to play with- WCK Programmer, Motion Builder, Action Builder, & Diagnostics Interface. RoboBuilder is ready to move as soon as it is assembled and using the software you can program your own humanoid motions in just 10 minutes. Another exciting feature is the ability to trade motion files on the internet uploading your own and downloading others. RoboBuilder is not only powerful, it’s affordable. You can choose from four kits priced at: $420, $680, $860, and $1,560.

The RoboBuilder kits are manufactured by RoboBuilder, LTD a Korean company: www.RoboBuilder.net. RoboBuilder is distributed by Trossen Robotics, LLC. More information about RoboBuilder can be found on the website: www.TrossenRobotics.com, 877-898-1005. Interested resellers are invited to contact them for more information.

Download the Press Release here.

Download the RoboBuilder Brochure here.

Interested resellers may call or email us for further information.

Summer Robot Sale!

Monday, July 14th, 2008

Our robots are dying of hot summer heat on our stuffy shelves! We need to get them to your air conditioned houses! Save a robot! Give one a home!

To encourage your adoption we are having a summer sale while supplies last. Let a robot into your heart and be a happier person.

 

 

 

i-Sobot by Tomy
 
Regular: $199.99
Sale Price $159.99
***SOLD OUT***
     

 

Kondo KHR-2HV
 
Regular: $939.00
Sale Price $798.15
***SOLD OUT***
     

 
Kondo KHR-2HV Starter Kit
 
Regular: $1,478.99
Sale Price $1,257.00
***SOLD OUT***
     

 
Kondo KHR-1HV
 
Regular: $1,249.99
Sale Price $1,062.49
***SOLD OUT***
     

 
Futaba RBT-1
 
Regular: $1,379.99
Sale Price $1,173.00 
***SOLD OUT***
     
     

 
VEXplorer
 
Regular: $199.99
Sale Price $179.99
     

 
Selected Pololu Controllers
     
Don’t forget that our garage sale section
also has ongoing deals for many items that are still in the box. Close
out, clearance, and discontinued items are in there all the time.

Want to get paid to play with robots?

Friday, July 11th, 2008

We are hiring !


Are you into robotics or similar technology? Do you have servos lying on your kitchen table? Does your office look more like an electronics lab? How about getting paid to play with robots? We have two open positions for enthusiastic individuals.

(Click job title for full description)

Technical Writer / Online Content Manager

Intern – Office Clerk / Warehouse

As we continue to grow we are always keeping our eyes open for good talent. Even if you don’t fit for one of the above positions you can send your resume in for future consideration. Some of the areas include: Ecommerce systems management & development, web design, marketing, Technical Support, Sales, and general operations.

Interested applicants can send their resumes & cover letter to Matt:

Surveyor SRV-1 gets facelift, more motors

Tuesday, July 1st, 2008
Surveyor SRV-1
Surveyor SRV-1: The Front!

Here’s a picture of the new Surveyor SRV-1 chassis, which is replacing the last version.  As you can see, the electronics are the same, but everything is recessed into the body now, which looks pretty slick.  The front plate that the laser pointers mount into also comes up to cover up the camera’s PCB.

The biggest differences are far from cosmetic, though.  The tracks are now driven by four motors instead of two.  Those of you with extra deep-pile 1970’s-era shag carpeting (we know you’re out there) don’t have to worry any more.  Surveyor Corp heard your call and answered it.  Backing up this quadruple-whammy of a drive system is a 7.2 V, 2000 mAh Lithium Polymer battery pack.  The new battery pack (a welcome upgrade from the older model’s bulky Li-Ion cells) boasts a runtime of 4 hours!

Surveyor SRV-1
Surveyor SRV-1: The Back!

GUESS WHAT. We sell these things, too.  If you’re planning a project that will require a number of small autonomous or wirelessly-controlled rovers, you don’t need to spend precious development time designing the bots!  The SRV-1 is a great out-of-the-box platform for swarm or solo applications; or any time you find yourself in need of a camera-equipped, Wi-Fi-enabled, internet-controllable, compact track-bot with a powerful main processor an killer battery life!

For development journals and all of the latest software updates, check out the Surveyor web site.
To see more detailed specs, or to purchase the robot, go to our Surveyor SRV-1 product page.