Codeshare Agreement Between Airlines

Code-share agreements are an important detail for flights to the EU when it comes to a right to reimbursement under EU Regulation 261/2004. But don`t worry. In this guide, we talk about code sharing and interline agreements. First we will describe what exactly it is. Next, we`ll discuss how you can determine whether or not you`re using code sharing. Finally, we show you why you should be interested in code sharing. Start. In this sense, I often get questions from readers who want to explain the difference between these different agreements, so I thought it would be fun to do so in this article. Before I do, I would like to add two exclusions of liability: code-sharing dates back to the 1960s. In 1967, Allegheny Airlines (later USAir) entered into the first codeshare with a commuter company in the United States.

Under the U.S. Domestic Market Deregulation Act in the 1970s, this practice became more popular. Passengers benefit enormously from codeshares and line spacing lines. In addition to cheaper tickets, you don`t have to worry, among other things, about the lack of air connections or the discovery of your luggage at each intermediate airport. Passengers can enjoy elite benefits and earn miles where they wouldn`t normally be able. Hot Tip: One of the best ways to tell with a reasonable level of accuracy that you are on a codeshare flight is if the flight number format does not match similar flights from the same company. Parallel operation is when two airlines use the same route and use the codes of the other than their own. If you know that your flight is a codeshare flight, you should find out as soon as possible who the exporting airline is. If you fly in business or first class, you will undoubtedly find a different product than what you booked at the beginning. Customers can buy a ticket from 1 airline, but travel with a number of other airlines as long as the airlines have a business relationship called a codeshare agreement.

As a result, customers have greater autonomy in choosing their flight plan, whichever suits them best. This flight is identified as an American Airlines flight “AA125”. What you will see is that long-haul flights are very rarely marked with 4 numbers. This is typically 1 or 2 numbers or 3 at most. If you find the format “XX1234” on an international flight, you are most likely on a codeshare flight. The exact operation of this revenue participation agreement depends on the specific agreement, but the idea is that two airlines essentially act as one in a joint venture. While it`s easy to understand that Allianz airlines retort elite benefits through Star Alliance, Oneworld or SkyTeam Elite status, the same is not true for other airlines. unless you`re on a codeshare flight…

Comments are closed.