This is my code in which I transmit the data to the bapi. I have a problem with the Bapi. this bapi is not executed in se37. Divisions are not generated. Could you please tell me what data this bapi needs and how to get this data by getting this data bapi_schedule_maintain.? – I don`t do it. With SAP S/4HANA Logistics` LoB sourcing and procurement system, SAP`s best practice activation approach can be used to customize delivery plans. However, if you use the traditional approach of customizing, this blog post can be helpful. Those who work with the traditional approach to customize delivery plans in SAP know that setting types and categories as well as maintaining output profiles can be difficult if you don`t know what you`re doing. The above information should be a reminder for those who are in the acquisition and introduction for those who started with SAP. I have a problem with. I am trying to change the WEBAZ field for the ME32L transaction, but although the bapi is successfully executed there and the message `Scheduling agreement 55500003590` is changed, it will not be changed. sap.ittoolbox.com/groups/technical-functional/sap-dev/bapi-or-fm-to-update-scheulde-lines-279080 planning agreements are defined and managed as supporting documents in the system. It is possible to group these documents into different types of documents according to commercial requirements.
First, you need to define the types of document and their attributes when adjusting. In this step, an exit profile for delivery plans is managed with a certificate of authorization. This profile determines the execution strategy and how delays and immediate requirements are taken into account when implementing. To maintain the exit profile, go to IMG (SPRO) > Materials Management > purchase > planning contract > manage SA`s establishment profile with the sharing document. I am looking for a BAPI or a functional item to update a delivery plan for a purchase schedule agreement. I saw in the threads a proposal on the use of BAPI_CONTRACT_CHANGE. However, we are at 4.7 and BAPI does not exist. I`ve tried using BAPI_PO_CHANGE, but it will be an error message that says it can`t be used for delivery plans. In addition, only the header BAPI_AGREEMENT_MAINTAIN updated… I want to know the bapi to create the divisions in me38.
I use bapi `BAPI_SCHEDULE_MAINTAIN`. But if I run this bapi, it gives me the 55000000188 instance agreement of the type of object purchschedagreement has been modified and the appointment agreement 5500000188 has been changed. However, the plan lines are not generated. Can you tell me what data I should give this Bapi and how I can pass it on to this Bapi? Can you please give me an example of code with this bapi, which is run correctly and generate divisions in me38? There is no Bapi to modify contract services, only bapi available for the creation of contract services (BAPI_AGREEMENT_MAINTAIN). Please leave for BDC. Yes, I used BAPI_TRANSACTION_COMMIT after using bapi_schedule_maintain, but no division is still generated. Can I insert my code here? Then you`ll understand. CALL_BAPI. Clear wa_header. IF sy-subrc NE 0.
CALL_BAPI2. Endif. DATA: ls_cont_hdr_in TYPE bapisdhd1, ls_cont_hdr_inx TYPE bapisdhd1x, lv_salesdoc bapivbeln-vbeln-vbeln, lt_return TYPE TABLE OF bapiret2, lt_partner TYPE TABLE OF bapiparnr, lt_item_in TYPE TABLE of bapisditm, lt_item_inx TABLE TYPE OF bapisditm, lv_msg TYPE There is no commit in se37. In other words, the commit fm bapi is not run, so you can`t be sure that the data will be recorded. It is therefore rare that there is a reason to test BAPIs in se37. I`m looking for a function/bapi to create hardware delivery plans in SAP. I think BAPI_PO_CREATE1 only orders. Are there any ideas on how you can create delivery plans by function? After setting the types of documents for delivery plans, select the line for the type of document and double-click on Authorized Item Categories. Manage on the screen Categories of items allowed for The category of articles, as shown in the following table.