HR-OS1 with Jasper Installed

Jasper Installed

Youtube User panthallion has installed Jasper on his HR-OS1 (with Raspberry Pi), and it’s pretty cool. The age of robotic personal assistance is upon us. Jasper is an open source platform for developing voice-controlled applications, similar to Siri, OK Google, Cortana, and so on. In this case, Jasper is being used in conjunction with an HR-OS1 to make a robot that can assist you with daily tasks, answer questions, tell a joke, and generally be responsive and helpful when given a voice command. It’s interesting to see the HR-OS1 physically reacting to the content it is delivering (it genuinely seems frustrated with one of the questions asked of it). Very clever!

Leave a Reply