Archive for November, 2015

DynamixShield Kickstarter!

Wednesday, November 18th, 2015

DynamixShield

Our friend at NeuroRobotic Technologies has been developing an Arduino Due Shield that plays nice with everything in the InterbotiX and RobotGeek product lines (and subsequently, his PhantomX Hexapod is playing nicely with the kids)! This is a comprehensive shield that lets you connect AX, MX, and XL Dynamixel Servos! The DynamixShield is an electronics board that fits onto an Arduino Due microcontroller to give you the ability to control Dynamixel smart servos and regular servos, while also providing numerous Grove and RobotGeek connectors. Grove and RobotGeek are hardware frameworks for modular sensors and actuators. There are tons of off-the-shelf modules for these two frameworks that can be plugged into the shield with a single cable. This includes everything from GPS sensors, RFID scanners, and LCD displays that are plug-and-play ready for use with the shield. This makes it very easy to build your robots by combining modules and servos. Check out his Kickstarter, and if you want to see it happen, you can make it happen!

We’re on Instructables!

Monday, November 9th, 2015

RobotGeek RFID Kits

We’ve got a few projects up on Instructables now! The newest of which is the RFID Windows Login Project! To celebrate, all of our RobotGeek RFID kits are on sale through November! Check it out!

Drinkinator Lives!

Wednesday, November 4th, 2015

Drinkinator

This project is so cool. Next Project Awesome has been working on a drink serving project known as Drinkinator. Utilizing a load of RobotGeek Pumping Stations, a Geekduino, and operated by a Raspberry Pi touch screen interface made in Kivy, this beautiful project makes for a fantastic automated party bartender. This project is well documented on Next Project Awesome’s GitHub, so if you’re looking for a project to follow, it doesn’t get much better than this. Next Project Awesome is an ambitious new youtube series that covers the use of Raspberry Pi and Arduino to make projects. They’re pretty amazing so far, and if you like what you see, you should subscribe to their channel!