Forum User r3n33 is at it again, this time with a new way to move the HR-OS1! WinRME is a .Net application that’s capable of relaying all the standard RME commands to the robot via manual entry, as well as a growing list of features. Based on RME (netRME), this program is shaping up to be a fantastic companion to the HR-OS1 for anyone using the Windows OS environment. This is exciting news. WinRME is being designed with a graphic user interface (a major improvement on the original), and will utilize multiple windows to allow you to keep your movement list on hand and ready to rock (a massive improvement on a personal pet peeve). There isn’t a download version available just yet, this is still in early development, but it’s worth checking out the screenshots below and following the forum post for more details!

WinRME Teaser Screen GrabWinRME Preview 2WinRME RoboPose Default ViewWinRME RoboPose Safety LimitsWinRME PoseManager

Leave a Reply