Archive for May 1st, 2015

RTEAM’s new Mech Warfare Robots!

Friday, May 1st, 2015

rteam

RTEAM Robotics Club from Tuscon, Arizona has been expanding their army of Mech Warfare combatants! Currently, they are testing out the use of Piezoelectric Speaker Scoring Panels instead of the FSR panels that have become a standard lately. This came about due to the expansion in number of mechs, and a lack of materials for half of them. User giantflaw offered some insight as to the continued use of Piezoelectric Speaker Scoring Panels:

RTEAM piezoelectric target plates are fully compatible with the existing target plate system and I think offer 6 advantages over the FSR plates. 1.) They are much more sensitive than the FSRs 2.) They register target plate hits reliably every time and never resgister any robot vibration or shock to the robot. The target plates are oblivious to walking gait. 3.) They are much cheaper than FSR target plates and easliy made with analog components. 4.) They can be de-tuned to be less sensitive and mimic an FSR low sensitivity target plate. 5.) There are no dead zones in the target panel like there are on FSR target panels. 6.) The target panel can be any shape or size unlike the FSR target panels. 7.) The target panels are tougher than the FSR plates and are not easily damaged.

If you’d like to see what the buzz is all about, hop in on this thread!