There are 2 new DYNAMIXEL PROs ready for order – the H42-20-S and the H54-200-S . Along with the H54-100-S , the entire line of ‘H’ series DYNAMXIEL PROs are available. These three servos sport some serious torque (5.6 – 39.131 Nm) and some amazing resolution (304,000-502,000 steps/turn).
In addition to the new servos, ROBOTIS has released 8 new frames for the DYNAMIXEL PRO line. Now it’s even easier to build around the DYNAMIXEL PROS!
Call us at 1-877-898-1005 for pricing and delivery information on the DYNAMIXEL PROS.