RFID is an exciting new technology that is finding its way into a variety of different industries; pet identification, keyless entry, hospitals, inventory management and tracking, tollway collections, security, data collection, wildlife tracking, and much more.
Beyond that, RFID is just plain cool and fun to play with. RFID has found its way into many DIY and interactive art projects over the last few years as people experiment with the possibilities of the technology. Now anyone can learn about RFID with this great RFID Experimenters kit.
This kit includes everything needed to get started:
- RedBee RFID reader
- RFID tag variety pack (13)
- Project CD with 5 Projects
- USB Cable
The projects disk comes with 5 great projects to do at home including RFID Login for your computer!
The 5 Projects Include:
- RFID Login (Windows 7)
- RFID Deadbolt
- RFID Safe
- RFID Racers
- RFID Logger (With database integration)

The RedBee RFID Reader is a ground breaking first in many areas. Capable of being used as a tethered device to a PC or microcontroller OR as a preprogrammed stand alone device it is the only hobby reader with both options. The RedBee also comes default with USB and TTL serial with the ability to add Xbee for wireless communication. Very cool!
Checkout the Huge feature list for the RedBee RFID Reader:
- Supports all EM41xx family 125 kHz RFID tags
- USB, XBee, and TTL Serial communication
- Serial Communication Protocol and Shared Serial Devices Protocol (SSDP)
- .NET programming API
- Operates as a slave device to PC or microcontroller
- Onboard programmable microcontroller
- Xbee point to point
- Xbee Mesh networking
- 3 power input options (Barrel Connector, USB, or Vcc)
- 4 Configurable I/O pins
- Valid/Invalid Tag LED
- Xbee Comm LED
Syndicate
Subscribe to this site's RSS feed.
Tags: Hobby RFID Kit, RedBee RFID Reader, RFID Experimenters Kit

Love the SSDP – is RedBee the only product that supports this?