Archive for December 11th, 2009

SMALdog, Sorta Maybe Almost Littledog

Friday, December 11th, 2009

If this robot looks vaguely familiar, it’s because it is inspired by Boston Dynamic’s LittleDog.

SMALdog, or Sorta Maybe Almost LittleDog, is Mike Ferguson’s (creator of the Arbotix Robocontroller) latest addition to his AX-12+ based quadrapod robot lineup.


Rather than utilizing the more common ‘lizard-style’ leg configuration, SMALdog has a more ‘mammal-style’ leg configuration that provides some interesting walking gait variations. The biggest difference is even with very little gait programming done so far, it’s already faster than the award winning Issydunnyet quadrapod. There is still a lot of work to be done on refining the walking gait, and the turning gait is barely functional, but this platform certainly shows promise. Check out Mike’s thread for more information and updates!