Archive for December 15th, 2008

Big Blue Saw’s End of the Year Sale!

Monday, December 15th, 2008

Our friends over at Big Blue Saw are having another sale, which is pretty much a dream come true for Roboticists building their own bots. They are generously offering discount quantity pricing on as little as single part orders, which means major savings for anyone looking to get custom work done for their projects. If you’ve ever looked into machine shop pricing you’ll know what a fantastic deal this is, you won’t find pricing like this anywhere so be sure to check them out! Founder Simon Arthur explains the details:

Big Blue Saw’s latest sale starts Tuesday, December 16, 2008 and ends Tuesday, January 6, 2009.

With this sale any aluminum 6061 parts of 0.1 inch or 0.063 inch thickness are automatically automatically eligible for a quantity discount — even on orders of as little as one part!

This is an excellent opportunity to try our services — you can order just one small part, and save on the setup charges.

This offer is valid for orders placed through our online ordering system only.

About the materials

Aluminum 6061

One of the perennial favorite materials at Big Blue Saw, the 6061 alloy of aluminum features excellent strength and light weight. It is weldable and has good corrosion resistance. This alloy is a true “aircraft aluminum”. Among many other applications, it was chosen by NASA to construct the crew cabin of the Space Shuttle.

MechRC Humanoid Back in Stock!

Monday, December 15th, 2008

When we first announced that we had the MechRC Humanoid Robot is in stock and ready to ship, they flew off the shelves almost instantly selling out. We now have limited quantities back in stock and are shipping out immediately, just in time for the Holidays! These won’t last long, so if you’re still looking for a great robotic gift for a loved one or even yourself, pick one up quick!

We’d also like to share this awesomely over-the-top promotional video: