Lego Wall-E, Geek-Envy is a cruel mistress

I used to pride myself as a Legos whiz. I had two entire trashcans full of them growing up and I could build ANYTHING. I even built a thermonuclear detonator out of my Technic set until the government decided that was too much power for one 11 year old to wield.

Well, today I hang my head in shame. My self proclaimed Lego genius has been shot down and put to shame. Bazmarc from our Community Forums has shattered my fragile ego, and shown us he is in a league of his own in Lego Supremacy. Behold the Lego NXT Autonomous Wall-E Robot! Seriously, this has to be the most impressive Lego robot we’ve seen yet, not only holding true to the likeness of the beloved Wall-E, but also boasting a feature set that would make the Ultimate Wall-E toy jealous.

Here are a few pictures of NXT Lego Wall-E (Click to Enlarge)

NXT WallE

WallE Guts!

Here’s a video of the little guy in action:

Share and Enjoy:
  • Digg
  • del.icio.us
  • description
  • ThisNext
  • Google
  • Live
  • NewsVine
  • Reddit
  • Slashdot
  • SphereIt
  • StumbleUpon
  • Facebook
  • LinkedIn
  • MySpace
  • TwitThis
  • Yahoo! Buzz

11 Responses to “Lego Wall-E, Geek-Envy is a cruel mistress”

  1. [...] [Trossenrobotics] VIA [Botropolis] TAGS: autonomous, lego, NXT, robot, Wall-E [...]

  2. [...] Mindstorms NXT. Ahora considero que es imposible vivir sin tenerla. Y es que después de ver el Wall•E fabricado con piezas de LEGO Mindstorms completamente animado y autónomo, las ganas de tener este producto se han incrementado una galaxia [...]

  3. [...] necesitas saber más, puedes visitar la web del autor o su álbum de [...]

  4. [...] Trossen Robotics members Bazmarc has created this Lego version of Wall-E.  Check out more pictures and a video over at Trossen. [...]

  5. [...] Cool Mods – Lego NXT Autonomous Wall-E Robot Posted 12 Sep. 2008 in Mods by Fatgadget Check out this cool Lego Wall-E robot built by bazmarc from the Trossen Robotics Forums. [...]

  6. [...] Check out th&#105s cool Lego W&#97ll-E &#114obot bu&#105lt b&#121 b&#97zm&#97rc fro&#109 th&#101 Trosse&#110 Ro&#98otics Forums. [...]

  7. [...] for visiting! Check out the amazing Lego NXT Autonomous Wall-E Robot built by a member of the Trossen Robotics Community [...]

  8. wow thanks Andrew, that’s a very sweet article you wrote on my LEGO Wall-E NXT. There are a lot of LEGO genius out there believe me it’s tuff to keep up, but i’m proud to be considered as one of them thru this project. I hope to dazzle you again with my upcoming projects!
    Marc-A aka bazmarc

  9. [...] robotics bloggers considered it a challenge. This LEGO blogger/robotics fan decided to just build his own LEGO Wall-E with electronics (proving my point [...]

  10. Emilie says:

    hello bazmarc
    Did you also provide the code that the Wall-E NXT robot was programmed with? Is it in NXT-G? Do you think you could post the code somewhere for anyone who wanted to try and build this?
    cheers,
    emilie

Leave a Reply