We have some exciting news for all of you fine people who have been calling us up over the years asking why there isn't an inexpensive plug-and-play solution for controlling stepper motors from a computer. Phidgets has just released the PhidgetStepper Unipolar 4-Motor controller! This little board, which is retailing for just $72.74, allows you to control up to 4 unipolar stepper motors from your USB port. Building a CNC rig? Building a wheeled robot that will need fast, precise speed and position control? Buy this controller.
From the official press release:
|
Phidgets adds a $75.00 stepper controller to its line of motor controllers The 1062 – PhidgetStepper Unipolar 4-motor, can control up to 4 stepper motors. CALGARY, Alberta, April 29, 2008 ― Phidgets Inc. today announced the addition of a new product to its family of motor controllers. The 1062 Stepper controller controls the position, velocity and acceleration of up to 4 unipolar stepper motors. Applications that require precise The 1062 plugs directly into the computer’s USB port and comes with a USB cable. Like all Phidgets, application programs can be written using the Phidgets API. “The 1062 Product Manual’s Technical Section contains valuable information and programming tips on how to “We already offer Servo controllers, and a variety of DC motor controllers. The arrival of a stepper controller fills a void in our family of motor controllers. ” says Chester Fitchett, CEO of Phidgets. “We have paid close attention to costs in order to give our customers the value/price ratio they are expecting from Phidgets.” added Fitchett. Product Specifications “Unlike a lot of our competitor’s products that require their users to write some firmware code in order to use their sensor, we are completely “Plug and Play” says Bernard Rousseau, Director of Marketing. “With Phidgets, you plug it in and start using it and when it comes to programming, the user, not us, decides which operating system and which computer language he wants to use”, added Rousseau. Users can program Phidgets using a simple yet powerful and well documented Application Programming Interfade (API) that is supported under Windows (2000, XP, Vista), Windows CE, Mac OS X, and Linux. Users can write programs in Visual Basic, VB.NET, C#, C/C++, Flash/Flex, Java, Labview, Matlab, ActionScript 3.0, and Cocoa. Phidgets also provides programming examples for all its products to help programmers write their own programs. The API Libraries as well as the examples and the documentation are available at no charge on www.Phidgets.com. |