Eric (aka Droid Works) has posted about an exciting new robot called RoboPhilo that is aiming to be under $500.
RoboPhilo was designed by RoboBrothers, Inc. USA and co-developed with the World Models Manufacturing Co. We talked with them and they said they are shooting to have the robot available by the holiday season. There is a gap of mispriced humanoids in the market and RoboPhilo may be the answer many entry level roboticists are looking for. We will get a sneak peak at the robot next month at the iHobby show. We will be sure to bring back some pics and videos for everyone.

Some Stats from the website
Name: RoboPhilo
Height: 13″ (330.2mm)
Weight: 1.2Kg (1200g) with battery
Included:
- PCB unit
- 36KHz controller
- 36KHz receiver
- 6V Ni-MH battery
- 7.2V 1000mA charger
- Graphical motion editor software
- Hanger Stand
Here is the official RoboPhilo website. Information is scarce as of now, so stay tuned for more info during the fall.

Thanks for the heads up Eric!
UPDATE: We now carry the RoboPhilo!









OK, it’s November, and the Robophilo web site is still mostly nonfunctional. Are they having production problems, or what? (Sorry for my impatience, but it looks too cool, and Christmas shopping season is upon us…)