Archive for July, 2007

New PC Based Robot Base?

Wednesday, July 18th, 2007
question mark

It looks like Rogue Robotics is coming out with a PC Based Robot Base. We couldn’t find any solid information about this base, but we’ll keep you posted when we find something out.

Futaba RBT-1 Humanoid Robot Unboxing Extravaganza!

Tuesday, July 17th, 2007

A few months ago, I announced the impending arrival of Futaba’s RBT-1 humanoid. Well, today I’m very pleased to tell you that it’s here! It’s in our shop, right in front of me, glaring menacingly with its glowing green eyes while it practices its Robo-Fu. So without further ado, here it is: the Futaba RBT-1 Unboxing Extravaganza!

Boxy goodness
There it is. Boxy goodness. Click for big.
Opening
Opening… Opening…
in the box
The goods, in the box. Click to enlarge
on the floor
The goods, on the floor. Click for a significantly larger version

Ok, now let’s talk about the goods. Taking a look at the picture above, we see the following items: the CD, some docs, the mighty RBT-1, serial cable, Li-Ion charger, AC adapter for charger, AC power cord for AC adapter, a Playstation-style controller, a nice little 7.4V 780mAh Li-Ion battery, and a tiny screwdriver. Now to assault you with information.

The Bot, At a Glance.

The RBT-1 from Futaba is slick, compact, and flexible. It stands just under 10 inches tall, yet still possesses 20 servos. The servos are small, but they are very quick and have an impressive turning range. They are serially controlled, with multi-port serial bus modules mounted on various parts of the robot, to split the signal off to the various actuators. The electronics are mostly inaccessible. I know there’s a tilt sensor in there somewhere, but it seems like it doesn’t really affect the pre-programmed motions, except to let the bot know that it’s lying on its back. This is something that will have to be explored further.

Our little robotic friend is controlled by a Playstation-style controller, with a motion sequence mapped to each button or joy stick. The moves assigned to the joy sticks can be executed proportionally to the position of the stick. For example, you can shift the robot’s weight variably using the right stick, leaning into turns or backing off to lessen the impact of a punch. Here’s a page from the manual, showing all of the pre-programmed moves and the buttons they’re assigned to:

popping and locking
Not quite popping and locking, but close.
As usual, click for high-res.

The chassis and joints have a notable feature as well. The servo horns are not rigidly attached to the frame pieces, as is the case with all of the other humanoid robots I’ve handled. Instead, the horn has a ring of knobs around its perimeter, which match to a ring of holes in the frame piece that it attaches to. What this amounts to is a a kind of clutch mechanism. If the joint is overstressed, the clutch will pop into a new position. This acts as a shock-absorbing system. If the bot takes a spill that would normally crack a bracket or strip a gear, the clutch kicks in and allows the joint to turn without damaging anything. Then it’s a simple matter of manually rotating the joint back into place. Sure, this could be seen as a weakness in high-impact combat situations, but I have the feeling that it will actually make the robot more durable in the long run, making up for the plastic brackets (which purists will inevitably complain about).

Software, At a Glance.

Futaba promised us some slick software, and it looks like they’ve delivered. Here’s a peek:

Motion Editor
Motion Editor. Pretty! Clicking graphic gets you bonus points for extra bigness.

I only got to mess around with this for a few minutes, but I must say I’m quite impressed. You can load up the canned motions and edit them, or start from scratch. Like many motion sequencing programs out there, it consists of picking joint positions, then defining transitions between them. There is a time line for organizing the steps in a particular motion, and also a “Scenario” timeline for stringing a sequence of motions together. Servo positions can be set in a number of ways. You can enter the angle in a text box or use arrows to increment/decrement said number. Also, and this is the fun way, you can just click on a joint in the nifty 3D view and swing the mouse around to reposition it.

Moving Pictures, Served Up Hot and Delicious.

RBT-1 shows off some moves:

Here’s a shot of me messing with the clutch-joints. They can be moved, but not that easily.

Oh, and did I mention we’re selling this thing? Well, WE ARE! Click here to purchase the Futaba RBT-1 Humanoid Robot. You’ll find more technical specs on the product page.

Robot Air Attack Squadron Bound for Iraq

Monday, July 16th, 2007

A turboprop engine powered airplane the size of a jet fighter capable of flying 300mph and reaching 50,000ft, isn’t too impressive for the US Military huh? Our military has more of them than we do items in our house. How about one that’s comes complete with infrared, laser and radar targeting with a ton and a half of guided bombs and missiles? Ok, this jet is getting a little cooler. Oh yeah, did I mention it is completely unmanned and that the pilot flies the plane while sitting at a video console in Nevada nearly 7,000 miles away?

Military Air Robot

Submit Your Project To Win A Gift Certificate

Friday, July 13th, 2007
Submit your project and WIN!
logo150
We want to know what you are building!
Every month the Trossen Robotics Team will evaluate the entries, and the top three most creative and/or useful projects will win a gift certificate:
July – August 2007* – Certificate to: Trossen Robotics
1st place – $100
2nd place – $50
3rd place – $25
To post your project go to Project Showcase in our forums.
Projects will be judged on the following criteria:
Wow factor - Just how much does your project make jaws drop? Do people gasp in glee at the bright lights and noises? Do they slap their heads at how brilliant the concept is? Your project can be either entertaining or everyday useful, either kind can have zing. The more zing the more bling in your pocket.
Smarty-ness - How brilliant is your project? Is it just sorta meh… or will it seriously pump up your geek cred? The more widgets, computers, code, and electronics involved the more you’ll score in this category.
Creative Spunk - How far did your mind have to stretch into the 4th dimension to come up with your project? Did you just invent another way to put the toilet seat back down, or is it so out there that it needed not one, but three flux capacitors? The farther projects are in the future, look like they belong in an art museum, or maybe should be safely kept behind glass, are point winners in this category.
Presentation, Documentation, & Explanation! - Don’t just send a single picture and a two line description; Your parents would be disappointed in you! Describe what you built. Take plenty of pictures. Take some videos (YouTube videos easily integrate into posts). Tell us what made you think of it. Tell us the parts you used and the problems you solved. Spend a little time documenting it so other people could duplicate the project if they wanted to try. Remember, this whole contest is about the community of DIY innovators showing each other great projects. People want to know the nuts and bolts of your creation.
~~~~~~~~~~~~~
Of course, you never know what we will and won’t like. The contest is subject to our whim and fancy and we can be a fickle bunch here at Trossen Robotics. Someone may create a donut flipper and we may love it just because they used our favorite donut in the video. Your spaceship was cool, but hey, we were hungry that day…
Good luck to everyone!
* July entries will be judged in August
** Entries will be eligible the month they are posted in. Trossen Robotics reserves the right to refuse award during any given month. All certificates are non-transferable and will not be accepted for cash.
“To have a great idea, have a lot of them.” — Thomas Edison

Different Colored Brackets For Robonova

Friday, July 13th, 2007

I was reading over some of the forum threads at Robosavvy, and one of their members pointed out that Hitec has updated their hitecrobotics site. I found some cool stuff in there; some old stuff and some I couldn’t recall if they had before. But, one new product that really stood out was different colored brackets for the Robonova. I’m sure that if I haven’t seen these before, many of our readers haven’t either, so I thought I’d share with everyone:

Robonova Colored Brackets

Getting a Humanoid to walk more “Human”

Friday, July 13th, 2007

Asimo, take some notes;)

Using 1930s theories from a physiologist by the name of Nikolai Bernstien, roboticists are able to build the world’s fastest dynamically walking robot!

Runbot is a small, biped robot which can move at speeds of more than three leg lengths per second, slightly slower than the fastest walking human.

Runbot

Bernstein said that animal movement was not under the total control of the brain but rather, “local circuits” did most of the command and control work.

The brain was involved in the process of walking, he said, only when the understood parameters were altered, such as moving from one type of terrain to another, or dealing with uneven surfaces.

How does Runbot walk you ask?

Runbot Gait

  • Frames 1 – 3: The robot’s momentum causes the robot to rise on its standing leg and a motor moves the swinging leg into position
  • Frame 3: The stretch sensor of the swinging leg is activated, which triggers the knee joint to straighten
  • Frames 3-6: The robot falls forward naturally, with no motor functions being used, and catches itself on the next standing leg
  • Frame 6: As the swinging leg touches the ground, the ground contact sensor in the foot triggers the hip extensor and the knee joint of the standing leg and the hip and knee joints of the swinging leg to swap roles

Read the full article via BBC News

Check out the creator of RunBot, Tao Geng’s page

Summer Sale at Trossen Robotics Through End of July!

Thursday, July 12th, 2007

So yeah… we were thinking. What could be the best way of thanking all of our customers and letting them know how much they’re appreciated.

Then the most obvious answer occurred to us: put on the biggest sale ever!

Good day robotics lovers!!!

Trossen Robotics is having a summer sale and would like to offer you a 10% discount on your next order!! This offer is good through July 31, 2007.

For more information, please click the link below:

Trossen Robotics Summer Sale

Thank you for your continued interest in our products and have a wonderful day!!

~ The Trossen Robotics Team

Star Banner

Next Gen Robot Researchers Dream of Humanizing Androids

Thursday, July 12th, 2007
Next Gen Robots
Professor Jimmy Or says he’s developed the world’s first self-supporting, walking humanoid robot with a flexible spine.

Household androids, like flying cars and Martian colonies, have disappointed generations of science-fiction enthusiasts by failing to materialize. Most research in robotics has drifted toward robots that, like Mars rovers and Roombas, have no resemblance to anything living, let alone human. And while it may be cute, let’s face it: Asimo can’t dance.

Bucking the trend, a small coterie of devoted professionals and amateurs are working to make fully articulated, humanoid and even sinuously dancing robots a reality.

Read the full article via Wired

RobuDog by Robosoft

Wednesday, July 11th, 2007

Robosoft’s newly announced robuDog packs quite a bit of pooch.

RobuDog

The robuDOG has been designed to bring news opportunities to researchers, teachers and hobbyists to investigate and develop advanced robotics solutions, as they can now program their robuDOG in the available 3D simulation environment , and then transfer this code for execution on the real robot dog.

Shown at RoboCup this past year and available later this fall, it has quite a nice assortment of features (taken from the robuDog pdf):

Platform:

  • Dimensions : 33×25x34 cm (LxWxH)
  • Weight : 3 kg
  • 17 joints (4 for each front legs, 3 for rear legs and 3 for the head)

robuBOX®:

  • Geode LX800 @ 500 MHz
  • 512 Mb + 2 Gb SSD
  • Wifi 802-11 b/g
  • Ethernet RJ-45
  • 1 x USB

Sensors and additional equipment:

  • 2D gyro
  • 2 infrared sensors
  • CMUcam3 : intelligent programmable color camera
  • Floor contact sensor on each foot
  • Stereo micro and loudspeaker
  • Li-po battery pack (4800 mAh)

Here’s a pic that Biodog posted in the Robosavvy forums that shows the feet and different colors available:

robuDog2

Hmmm… those servos definitely look familar. With all of the features of the Bioloid servos (not to forget 17 of them!) in addition to the robuDog supporting MSRS, I bet this pooch is going to be quite the impressive soccer player:)

This pooch is pretty slick, sure, but, is it worth the hefty, according to RobuDog’s product page, $4405 (3,200 €) price tag? If anyone has any info on this price, leave a comment!
via (Engadget)

Holy Moley, It’s Raining Old Computers!

Monday, July 9th, 2007
Wheeeeee!
Wheeeeeeee!!!

We (Trossen Robotics employees) are nerds. It’s required. It was a check-box on the job application. We spend a considerable portion of our waking hours working with and researching the latest in modern technology. In addition to digging the highest of the high-tech, we also have a deep appreciation for the history behind said technology. Here’s a site we like and we figured you’d like it too. The Obsolete Technology Website is not an exhaustive encyclopedia of computer history, but rather the collection of one quirky aficionado. He collects old PC’s, and he made a cool web site with details about all of the computers he has and some that he’s looking for. Ever heard of the Synertek SYM Model 1? Until a few minutes ago, neither had I; but now I know all about it! Learning obscure facts can make you appear to be an intellectually well-rounded person, at least to the casual observer! So what are you waiting for? Round yourself out with some sweet Obsolete Technology!