Futaba RBT-1 Humanoid Robot Unboxing Extravaganza!

A few months ago, I announced the impending arrival of Futaba’s RBT-1 humanoid. Well, today I’m very pleased to tell you that it’s here! It’s in our shop, right in front of me, glaring menacingly with its glowing green eyes while it practices its Robo-Fu. So without further ado, here it is: the Futaba RBT-1 Unboxing Extravaganza!

Boxy goodness
There it is. Boxy goodness. Click for big.
Opening
Opening… Opening…
in the box
The goods, in the box. Click to enlarge
on the floor
The goods, on the floor. Click for a significantly larger version

Ok, now let’s talk about the goods. Taking a look at the picture above, we see the following items: the CD, some docs, the mighty RBT-1, serial cable, Li-Ion charger, AC adapter for charger, AC power cord for AC adapter, a Playstation-style controller, a nice little 7.4V 780mAh Li-Ion battery, and a tiny screwdriver. Now to assault you with information.

The Bot, At a Glance.

The RBT-1 from Futaba is slick, compact, and flexible. It stands just under 10 inches tall, yet still possesses 20 servos. The servos are small, but they are very quick and have an impressive turning range. They are serially controlled, with multi-port serial bus modules mounted on various parts of the robot, to split the signal off to the various actuators. The electronics are mostly inaccessible. I know there’s a tilt sensor in there somewhere, but it seems like it doesn’t really affect the pre-programmed motions, except to let the bot know that it’s lying on its back. This is something that will have to be explored further.

Our little robotic friend is controlled by a Playstation-style controller, with a motion sequence mapped to each button or joy stick. The moves assigned to the joy sticks can be executed proportionally to the position of the stick. For example, you can shift the robot’s weight variably using the right stick, leaning into turns or backing off to lessen the impact of a punch. Here’s a page from the manual, showing all of the pre-programmed moves and the buttons they’re assigned to:

popping and locking
Not quite popping and locking, but close.
As usual, click for high-res.

The chassis and joints have a notable feature as well. The servo horns are not rigidly attached to the frame pieces, as is the case with all of the other humanoid robots I’ve handled. Instead, the horn has a ring of knobs around its perimeter, which match to a ring of holes in the frame piece that it attaches to. What this amounts to is a a kind of clutch mechanism. If the joint is overstressed, the clutch will pop into a new position. This acts as a shock-absorbing system. If the bot takes a spill that would normally crack a bracket or strip a gear, the clutch kicks in and allows the joint to turn without damaging anything. Then it’s a simple matter of manually rotating the joint back into place. Sure, this could be seen as a weakness in high-impact combat situations, but I have the feeling that it will actually make the robot more durable in the long run, making up for the plastic brackets (which purists will inevitably complain about).

Software, At a Glance.

Futaba promised us some slick software, and it looks like they’ve delivered. Here’s a peek:

Motion Editor
Motion Editor. Pretty! Clicking graphic gets you bonus points for extra bigness.

I only got to mess around with this for a few minutes, but I must say I’m quite impressed. You can load up the canned motions and edit them, or start from scratch. Like many motion sequencing programs out there, it consists of picking joint positions, then defining transitions between them. There is a time line for organizing the steps in a particular motion, and also a “Scenario” timeline for stringing a sequence of motions together. Servo positions can be set in a number of ways. You can enter the angle in a text box or use arrows to increment/decrement said number. Also, and this is the fun way, you can just click on a joint in the nifty 3D view and swing the mouse around to reposition it.

Moving Pictures, Served Up Hot and Delicious.

RBT-1 shows off some moves:

Here’s a shot of me messing with the clutch-joints. They can be moved, but not that easily.

Oh, and did I mention we’re selling this thing? Well, WE ARE! Click here to purchase the Futaba RBT-1 Humanoid Robot. You’ll find more technical specs on the product page.

15 Responses to “Futaba RBT-1 Humanoid Robot Unboxing Extravaganza!”

  1. Roland says:

    Hi,

    Is the RBT-1 expandable with other sensors or gyro etc ?
    Can it be programmed in other languages than the software shipped with the bot?

    greetz

  2. fuzzyoboe says:

    I got mine yesterday, the manual file (acrobat) on the CD seems corrupted. Is it only mine, or is the problem with every CD

  3. Dave says:

    Thanks for the comments!

    Roland: It looks like you can only program it using the proprietary software. However, I haven’t read through the manual completely, and I’ve only had an hour or so of hands-on time with the bot itself. I’m confident that if I don’t figure out how to hack into it, someone else will.

    As for the sensors, there is an expansion port on the controller. It has four pins and the manual says that it’s for a 2-axis gyro that is currently in development. This would lead me to believe that two of those pins are analog inputs, which could potentially be used for other things, but I’m not promising anything. Stay tuned for news as it develops.

    fuzzyoboe: Sorry to hear about that. I’m putting up a link to download the manual from out product page. If anybody has a corrupt file, or just wants to check out the goods before they buy the robot, feel free to download the manual from this page:

    http://www.trossenrobotics.com/store/p/5235-Futaba-RBT-1.aspx

  4. fuzzyoboe says:

    Thanks a lot. I downloaded the manual.

  5. Roland says:

    Thanks for your reply Dave!

  6. Dave says:

    For future reference: we do not receive automatic notifications for blog comments, so this isn’t really the best place to leave a tech support request. We check over the comments occasionally, but sometimes we miss a few. If you need help with something, please call or email us.

  7. Thavi says:

    Hey i kind of the the CD is there anyway for me to download the software??Or els i am just stuck with a robot -__-.
    Thanks

  8. Dave says:

    Thavi– Email me (davep@trossenrobotics.com) and I’ll send you a link so you can download the software.

    Also, let me reiterate my previous statement: If you need technical assistance, and this includes tracking down new manuals or software, please email a TR employee. This is the best way to get a prompt reply.

  9. Randy Peral says:

    Hello, I’ve noticed that in the PC requirements, it said windows 2000 or XP, has there been any upgrades for Vista? Please let me know, cause as of this Jan. I plan on purchasing the Futaba RBT-1 , I’ve already purchased an i-sobot, and it’s pretty neat and all for the price, but I must admit, from looking at the Futaba RBT-1 videos, I’m sure that I’ll enjoy adding the humanoid as my new hobby/ collection. Please, let me know about my question, it would be much appreciated, thank you.

  10. Randy Peral says:

    I’m sorry, 1 more question, does the Futaba RBT-1 only come in blue, or, can you still get it in black also.

  11. Alex says:

    The RBT-1 only comes in blue. As far as the PC requirements, I haven’t heard of any upgrades for Vista, but Dave is our RBT-1 expert. I’ll email him to check this out.

  12. Dave says:

    Unfortunately, I don’t know anything about RBT-1’s Vista compatability, present or future.

  13. Randy Peral says:

    Hello Team, it’s me again ofcourse with another ? For accessories, would you happen to know if there’s a carrying case available, and if not, will there be? I’ve noticed that the Robonova hac a carrier, and I thought it would be great if the RBT-1 would have one, let me know, thank you for your time, one more thing, it is because of you guys that has made me decide on picking up humanoid/ robots as a hobby, thank you very much, this has always been a dream for me since I was a little kid, but, unfortunatlely, because of lack of funds and the technology, I was not able to pursue it, again, thanks.

  14. Alex says:

    Nope, sorry no carrying case is available for the RBT-1, and I haven’t heard any talk of one:(

    Thanks for the kind words:) Robots were always my passion as a child too!

  15. kyle says:

    how long does the battery last and should i get an extra and/or the charger

Leave a Reply