Robot Air Attack Squadron Bound for Iraq

A turboprop engine powered airplane the size of a jet fighter capable of flying 300mph and reaching 50,000ft, isn’t too impressive for the US Military huh? Our military has more of them than we do items in our house. How about one that’s comes complete with infrared, laser and radar targeting with a ton and a half of guided bombs and missiles? Ok, this jet is getting a little cooler. Oh yeah, did I mention it is completely unmanned and that the pilot flies the plane while sitting at a video console in Nevada nearly 7,000 miles away?

Military Air Robot

Leave a Reply