Engineering life after robots


genpets

We are still engineering life in the form of robots, but after that is conquered we perpetually unsatisfied humans will certainly move onto other things. The next step after robots will of course be bioengineered life! How exciting. It looks like one company, Genpet, has already gotten a head start marketing their product line. Look out Ugobe, Pleo already has some competition!

Genpet Features !

Genpet_feature

01. Genpetâ„¢
The Only Bioengineered Buddy. Available in 7 different personality types.

02. Color Coding
Each personality type of the Genpets has been linked to its respective colour, and that color is then used as a base for each package. (Read more)

03. Heart Monitor
Each package has a built in low cost heart monitor that is fully functional, with green LED lights and built in speaker. (Read more)

04. Fresh Strip
Every single package includes an easy to use “fresh gauge”. Four simple blue LED lights display the status of the Genpetâ„¢. The display will also display if the Genpetâ„¢ has been sitting on the store shelf too long, or if the package circuitry has malfunctioned in some way. (Read more)

05. Bio-Genica IV System
While the Genpets hang on the store shelves they are in a form of hibernation. Each Genpetâ„¢ package has a special nutrient feeding tube attached to it, supplying our specially formulated mix and keeping them healthy and asleep.

06. Genpetâ„¢ Restraints
Restraining the pets in their packaging ensures no damage to the product, as well as allowing for optimal consumer viewing.

Visit their site today and get in line to order yours!

Gen-pet-wall

link

Share and Enjoy:
  • Digg
  • del.icio.us
  • description
  • ThisNext
  • Google
  • Live
  • NewsVine
  • Reddit
  • Slashdot
  • SphereIt
  • StumbleUpon
  • Facebook
  • LinkedIn
  • MySpace
  • TwitThis
  • Yahoo! Buzz

2 Responses to “Engineering life after robots”

  1. Bob Mottram says:

    This isn’t actually a real product, just a clever piece of artwork, but the fact that something like this seems believable at all is because we’re not too far off from being able to manipulate genetics in this kind of way.

  2. Alex says:

    nope, not a real product, but it is certainly an eye catcher, huh? It really makes all of us think about what sort of products may come out of the technology that is being developed and used today.

Leave a Reply