“KHR-1, the Japanese Robo-One humanoid robot kit from Kondo (previously mentioned here), is finally open for creative software development. The first unofficial implementation of the PC-controller API has just been posted. Using the SDK, the 17 servos that give the robot its mobility can be remote controlled by the PC via WiFi or bluetooth, and their current position can be retrieved several times per second. This unique feature will allow robot fans to go beyond simple performance of motion sequences or low-level gyro-based motion correction and develop algorithms that involve feedback control and AI.”
Via Slashdot Post